It looks like you are coming from United States, but the current site you have selected to visit is Moldova. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode
< View all Making Connections
Blog header images - MCS electric

A new era of utility excellence with the StratusĀ® Evolve intelligent grid platform

The electric grid is undergoing a massive transformation. Utilities face growing pressure from all sides: rapid load growth driven by electrification, the rise of distributed energy resources, and increasing customer expectations for reliability. Reading a meter just to check a box for billing isn’t enough to manage this complex, dynamic environment. A new digital approach is needed—one that turns data into immediate, actionable insights. 

This is where the new Stratus® Evolve intelligent grid platform comes in. It represents an innovative shift in how utilities can monitor, manage, and plan their operations. By moving beyond just measurement, Evolve helps you gain deeper insight, act faster, and build a more resilient grid for the future. It's time to transform your grid data into your greatest operational asset.

Shift from passive to proactive grid management

For decades, the electric meter has served a single, crucial function: measuring consumption for billing. While essential, this offers a limited view of grid performance. The Evolve platform redefines the meter's role, transforming it from a passive data collector into an active, smart grid sensor.

This change enables a move away from reactive problem-solving toward proactive, continuous system maintenance. Instead of only learning about an outage when customers call, you can get near real-time alerts. Rather than relying on modeling for voltage and load profiles, you can see actual conditions as they happen. This shift provides the granular data needed to make operational decisions with confidence.

Turning data into actionable intelligence

Utilities are collecting more data than ever before, but data alone doesn't create value. The key is turning that raw information into intelligence that supports your teams, from engineering to customer service. Evolve is a digital-first ecosystem built to bridge this gap.

The platform processes large volumes of data and delivers the full picture that helps you:

  • Dynamically manage the grid: Respond to changing conditions in real time, not after the fact. With higher data sampling rates, you get a clearer picture of system health, allowing you to optimize performance and prevent issues before they escalate.
  • Improve reliability: Faster fault detection is critical for minimizing downtime and improving customer satisfaction. Evolve provides the data needed to pinpoint problems quickly, reducing outage duration and enhancing overall grid reliability.
  • Plan for future capacity: As demand from electric vehicles and other sources grows, accurate capacity planning is essential. This platform delivers detailed load analysis, helping you understand usage patterns, and make informed investment decisions for future infrastructure needs.

Future-proof solutions for a changing energy landscape

The one constant in the energy sector is change. Regulatory requirements emerge, new technologies become mainstream, and customer expectations rise. A static solution can quickly become obsolete and cause expensive “rip and replace” upgrades. That’s why Evolve was designed as a flexible, software-based platform built for the future.

This forward-looking architecture provides several key advantages:

  • Continuous updates: The platform can be updated with new features and system-wide enhancements without disrupting daily operations. This ensures your investment continues to deliver value for years to come. 
  • Faster application deployment: Deploy new electric grid applications, analytics, and software solutions more quickly. This digital-first approach positions utilities to be agile to meet future demands. 
  • Customization and scalability: Evolve is built to scale with your operations. It supports utility-specific applications, allowing you to tailor the platform to your unique operational needs as you grow.
  • Robust communications: The platform builds on the proven Sensus FlexNet® communications network, designed specifically for utility operations, while also supporting complementary communications for increased resilience and reliability.

A more intelligent foundation for the modern grid

The challenges facing electric utilities are significant, but so are the opportunities. By embracing new technology and a new way of thinking about grid data, you can build a more efficient, reliable, and future-proof network.

The Evolve platform provides an intelligent, adaptable foundation needed for the modern grid. By transforming the meter into a powerful digital ecosystem, it enables you to move beyond billing-centric metering and toward a state of continuous operational awareness. It’s more than just collecting data; it's about turning that data into the timely, meaningful insights you need to serve your customers and manage your grid with greater confidence.

;