It looks like you are coming from United States, but the current site you have selected to visit is Moldova. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

Providing a System with Budget and Schedule Constraints

Evoqua works with a tight budget and delivery requirements to provide a system that met the semiconductor fab needs

Challenge

This semiconductor fab was challenged with a tight budget and an accelerated project schedule to meet production needs.

Solution

The original bid for this job included a new UPW system with turnkey services, however the final project required Evoqua Water Technologies to utilize existing equipment supplied in a building that was being shut down. The challenge was to reinstall this equipment at another site with a very tight turn around.

Evoqua supplied additional filters, UV sterilizers, pumps, and refurbishment of the existing equipment that was necessary to meet water quality requirement for the building, as well as provide a guaranteed system. The complete system includes pretreatment, reverse osmosis, service deionization, UVs and polishing filters.

Evoqua provided installation supervision services with the relocation and installation work being contracted directly with the customer.

Results

This project is a good example of how Evoqua Water Technologies can work within a customer’s tight budget and delivery requirements while still providing a system that meets their needs.