It looks like you are coming from United States, but the current site you have selected to visit is Montenegro. Do you want to change site?

Yes, please! No, keep me on the current site

Stratmoor Hills Expands Footprint To Mitigate PFCs

The district transitions from seasonal to year-round drinking water treatment, mitigating PFCs including PFOA and PFOS

Challenge

Since 2018 Stratmoor Hills Water & Sanitation Districts in Stratmoor Hills, Colorado has had two IX48 ion exchange treatment systems in place to remove PFOA and PFOS from two separate wells. Each treatment system was seasonal, running only in the summer and consisted of an ion exchange system from Evoqua Water Technologies. Each system treated up to 200 gpm or 250,000 gallons per day for 5 months, then was shut off and stored for the winter months. Stratmoor Hills Water & Sanitation Districts wanted to expand its treatment to include treating an additional well and allow the current system to be upgraded. The expansion would include a new treatment plant system using the existing IX48 systems along with two (2) additional new IX48 systems to run year-round, and a new climate-controlled building. The system would require treating up to 800 gpm or approximately 1.1MM gallons per day, removing PFOA and PFOS to meet Colorado’s state drinking water regulations.

As a foundation the project already had some necessary information it would need to move forward. The Districts already understood the water chemistry, based on its history of working with Evoqua, and it knew what the flow rate would be, based on its other wells.

One of the challenges to overcome would be Stratmoor’s new reliance on its own wells for year-round service and closing off its seasonal tap into neighboring Fountain’s aquifer, except when necessary.

"We may be the smallest water district in the area, but we are the leaders in removing PFCs to non-detect levels using state-of-the-art systems."
Kevin Niles, Superintendent, Stratmoor Hills Water & Sanitation Districts

Solution

The new system utilizes cartridge, ultraviolet and ion exchange filtration to provide up to 1.1MM gallons of treated clean, safe water per day to Stratmoor Hills residents.

Results

Customers of Stratmoor Hills Water and Sanitation Districts are receiving water that is compliant and meets the treatment goal of removing PFCs to current non-detect levels using Evoqua's state-of-the-art system.

"Our Centralized Treatment Facility is the crown jewel of our Stratmoor Hills Water & Sanitation Districts. We love that we can make the drinking water safe for our community, and we appreciate having Evoqua Water Technologies as our partner."
Nancy Lee Watkins, Field Supervisor, Stratmoor Hills Water & Sanitation Districts