It looks like you are coming from United States, but the current site you have selected to visit is Mongolia. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

How to select the right small-scale pumping solution for your application

Selecting the right small-scale pumping solution starts with understanding your application's specific requirements – from what you're pumping and how much, to how the pump will be controlled and where it will sit in your system. This guide covers the eight key factors you and your solutions provider should evaluate together before selecting a pump.

What will you use the pump for?

The first step in selecting the right small-scale pumping solution is to clarify its intended use. Will you be pumping, transferring, boosting, or spraying? Some specialty pumps are better suited for specific uses than others, and getting this right upfront shapes every decision that follows. Together, we can help you map your application requirements to the right pump configuration from the start.

What fluid or material will you be pumping?

Understanding what you're pumping is essential – the exact composition, temperature, and concentration of your fluid directly determines the materials your pump needs to be built from. This matters most for chemical compatibility: corrosion can cause leakage and failure, so soak-testing the materials before committing to a pump is strongly recommended. Your Xylem solutions provider can advise on the chemical compatibility of any pump for your specific application.

How does fluid viscosity affect your pump selection?

Viscosity, the internal resistance a fluid has to flow, is one of the more nuanced variables in small-scale pump selection, and it's worth working through carefully. In general, it describes the "thickness" of a fluid: water is thin with low viscosity and can be pumped at higher volumes and speeds, while oils are thicker and require lower volumes or pressures. Beyond fluid type, viscosity is also affected by pump orientation, pump speed, port size, and system pipework dimensions and length.

It's also worth noting that viscosity is highly temperature-dependent. High-viscosity fluids can sometimes be pumped more effectively with slight agitation, a gentle stir or controlled heating of the medium, but each material needs to be evaluated on its own characteristics before altering its viscosity for pumping.

What flow rate does your application require?

Flow rate – the speed at which you need liquid pumped – is one of the most important factors in choosing the right small-scale pumping solution, and it's directly shaped by your intended use. For spraying applications, nozzle size drives it. For transfer applications, optimal cycle time is the key variable. For dispensing, it's the volume required per cycle. In your application, if a range of flow rates is compatible, we always recommend specifying a lower flow rate as it extends pump life and improves long-term reliability.

How do head and pressure requirements determine pump power?

Head or pressure, combined with your flow rate, determines the pump power your application needs. When discharge is at a higher level than suction, pump power is calculated by the differential height between the liquid level on the suction and discharge sides. Pressure requirements can also be driven by flow through a nozzle, or by frictional loss through tubing and fittings at a given flow rate. If you're pumping into a higher-pressured vessel or from a vacuum, the differential between suction and discharge vessel pressures is also factored in. Always choose a pump rated for the pressure required in your system.

What pump control method is right for your application?

How you turn the pump on and off has a direct impact on pump life and it's a decision worth getting right upfront. For applications with a closed valve or a spray wand with a trigger, a demand pump with a pressure switch is the right choice: it shuts the pump off when the valve is closed, preventing the pump from running against a dead head, which can cause immediate failure in positive displacement pumps. For other applications, a bypass system protects against failure. More complex use cases may require sensors and electronic controls. We can help you think through the right control approach for your specific setup.

What power source will drive your pump?

The right driver for your small-scale pumping solution is generally determined by what's available in your system. For motor- or solenoid-driven pumps, you'll need to know the voltage and frequency of the power source – AC or DC governs the motor type, and oscillating pumps designed for AC cycling cannot operate on DC. If you have compressed air available and opt for an air-driven pump, you'll need to know the inlet pressure and how to regulate it. In flammable atmospheres, properly grounded air-driven pumps are recommended to eliminate explosion risk.

Does pump placement affect performance?

Where your pump sits relative to the liquid level directly affects priming and choosing the wrong setup can lead to dry running and early pump failure. A pump located above the liquid level, or without a flooded suction, always needs to be primed before operation. Most positive displacement pumps can self-prime but only within their rated priming capability. Exceeding that limit means the pump won't prime and will run dry, which causes accelerated wear and early failure if it occurs frequently. Getting placement right is one of the details worth confirming with your solutions provider before installation. 

These are the core factors to evaluate when specifying a small-scale pumping solution but other variables like duty cycle, ambient temperature, and plumbing configuration all have a bearing on performance too. We recommend working through these details with your Xylem solutions provider to confirm the specifications that best support your application.

When you're ready to select your small-scale pumping solution, Xylem's Flojet, Jabsco, and Rule brands are built specifically for the precision, reliability, and application versatility that specialized pumping demands. Together, we bring technical expertise and engineering to help you find the right solution whether you're optimizing an OEM design, replacing a legacy pump, or specifying for a new application. Let's work through it together. Contact us today to get a quote, ask a technical question, or connect with a solutions specialist.

FAQ: Selecting a small-scale pumping solution

What is a small-scale pumping solution? 

A small-scale pumping solution is a compact specialized pump engineered for lower-flow applications requiring precision, chemical compatibility, and specialized performance. Xylem's Flojet, Jabsco, and Rule brands are purpose-built for this category, serving OEMs and operators across industrial, marine, and food & beverage applications.

How is a small-scale pump different from a standard industrial pump? 

Small-scale pumps like those in the Flojet, Jabsco, and Rule families are engineered for lower flow rates, compact installation environments, and application-specific performance – not the high-volume throughput of large industrial pumps. This makes them the right choice when precision, portability, or specialized fluid handling is the priority.

What factors matter most when selecting a small-scale specialized pump? 

The most critical factors are intended use, fluid composition, viscosity, required flow rate, and system pressure. Together, these variables determine the right pump type, material of construction, and power configuration. Working with a solutions provider early in the process helps ensure everything is aligned before you commit to a specification.

When should I consult a solutions provider for pump selection? 

Any time you're working through chemical compatibility, system pressure requirements, or duty cycle constraints, we recommend connecting with your Xylem solutions provider. The variables in pump selection are interconnected, and getting a recommendation aligned to your exact application protects both performance and pump longevity.