-
-
-
Lowara pumps drive livestock operations
In a major breeding farm from Bergamo, Italy, Rota Guido Srl has installed two reverse osmosis (RO) and ultrafiltration plants that, coupled with a biogas plant ensure local livestock operations are efficient, sanitary and environmentally responsible.
-
-
-
-
-
Leather processing hots up with new Lowara e-SV for high temperature applications
The new e-SV ”Boiler” 180°C can pump water at 170°C for 12 hours continuously without the need for regular external maintenance such as mechanical seal cooling, which is of enormous benefit to the customer.
-
-
-
-
Goulds Water Technology rainwater for today’s high water demand households
In the remote dry Southwest, where water scarcity and escalating demand are daily issues faced by homeowners, third generation Goulds Water Technology professional Kevin Cunningham is finding new uses for Goulds Water Technology variable speed and constant pressure systems.
-
Rodeo’s demands for irrigation and feeding
Agriculture is by far the largest user of water – up to 70% of all fresh water consumption is for irrigation. Water has many other agricultural purposes such as washing stations, misters, or drinking water for livestock. In fact, horses consume up to 15 gallons of water per day.
-
Pumps built to stand the test of time
When Paint/Elk Township Sewage Plant installed a Goulds Water Technology submersible effluent pump in the spring of 1991, they would be set for the next two decades.
-
Xylem helps to save the Sphinx and Giza Pyramids
To solve the groundwater problems, the EAA and United States Agency for International Development created the Pyramids Plateau Groundwater Lowering Project. Hydrotech evaluated the project and selected Xylem’s Goulds Water Technology products as the best solution for the groundwater problem.
-
D&S Pump Supply and Goulds Water Technology keep Quaker Hill Country Club in the green
Over time, the irrigation, pressure boosting and flow control systems at Quaker Hill Country Club became problematic and the grounds crew was only able to water one green or fairway at a time. The possibility of a pump failure forced the staff to monitor the pump continuously while in operation to ensure they shut it down before it ran dry.
-
It’s elementary – Xylem goes to the ‘head’ of the class
The best solution for an elementary school in New York was to install two Goulds Water Technology Hydrovar® variable speed frequency drives (VFD) mounted on the existing 5HP SSV Pumps. Selecting this system would provide the constant pressure needed, enhance efficiency, reduce operation and maintenance costs and decrease space requirements.
-
Galen Glen Winery bears fruit with selection of Goulds Water Technology products
Located in the rolling hills of eastern Pennsylvania, Galen Glen produces award-winning, handcrafted red, white and sparkling wines. However, in order for the vineyard to grow grapes in this environment, a reliable water source is required to supplement the rainfall.
-
-
-
Bucknell University selects Goulds Water Technology as first in class
Bucknell University implemented a new pump system with variable frequency drive controls to monitor flow and response and increase the output of the pump to keep up with the fluctuating demands of the three different buildings.
-
Pennsylvania campground a perfect destination with Goulds Water Technology solution
Since swimming pools and shower facilities are important considerations when campers are selecting a destination, StoneyBrook Estates Campground wanted to ensure that its 30,000-gallon swimming pool and shower house were functioning effectively and efficiently.
-
Goulds Water Technology teams up with customers to provide reliable water source to a Connecticut community
The Catskill Mountains make for beautiful scenery but the rolling hills present the challenge of reliably pumping water to residential areas. Xylem’s Goulds Water Technology Aquavar Intelligent Pump Controller, and the help of distributor D&S Pump and Supply Co., and installer Foley’s Pump Service ensure water reaches a Connecticut community.
-