It looks like you are coming from United States, but the current site you have selected to visit is Oman. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

Enhancing the Wastewater Treatment Process for the foreseeable future

January 12, 2021

Johannesburg, 12 January 2021: Though the dangers of waste products, such as disease, only became evident over time, ancient societies long tried to manage the problem. For example, the Ancient Greeks built covered sewage systems, some of which still operate today, 4,000 years later. Romans, the Indus Valley people, and China’s Northern Song Dynasty all made breakthroughs in the ancient waste management world. But it was only around the rise of industrialisation, such as London’s Bazalgette sewer system from the mid-1800s, that modern wastewater management became a concept.

We have learned a lot since then, explains Chetan Mistry, Strategy and Marketing Manager for Africa, “There’s no doubt that modern sanitation practices have created a better world. There is less disease, cities are no longer dangerously septic, and clean water is something available to most people on the planet. But there are still many improvements that we can make. For example, the idea of pollution dilution is completely outdated.”

Not everything disappears in dilution

Pollution dilution was, at face value, a sound idea for its time. It holds that waste such as affluent will become harmless once introduced into much larger bodies of water. But it’s insufficient, bad for the environment, and potentially very harmful to humans.

“We’ve become much more aware of what is in waste. As detection methods improved, the world learned that waste contains previously undetected things such as medicinal waste, microplastics, endocrine plastics, and hormone disruptors. These types of waste are not diluting in the ecosystem, nor do they need large quantities to be a risk factor for humans.”

There is growing acknowledgement that it’s not wise to pump waste, treated or otherwise, into our water systems - especially when you look at how much more urbanised and densely populated our cities are becoming.

These newly discovered types of waste need tertiary steps to remove, often mandated by national and international laws governing the quality of water. Underpinning those efforts, and driving more efficiencies for water treatment, are monitoring, measurement and tracking technologies.

Improvement Wastewater Treatment

The standard wastewater cycle, in broad strokes, requires the removal of grit, sand, organics, large objects, and creatures such as bacteria. New types of waste add to those processes. This is an opportunity to systematically improve all of the treatment cycle, through the following elements:

  • Better tracking and measurement - It is much more feasible and cost-effective to introduce sensors into a treatment facility, monitoring factors such as affluent flow and maintenance requirements. The cost of sensor systems is so low that the payback of such investments can be as little as 2 to 3 years. Operators and managers have access to dashboards and alerts to look at every aspect from one view.

  • More visibility and control - Dashboards combined with sensors create increased visibility of a facility. Current modernisation takes it a step further. You could typically expect to get facility information at the facility. But what about remotely on your phone, including the ability to change schedules or start/stop pumps even if you’re not on-site? These capabilities sit at the heart of modern facility management technologies.

  • Optimisation through analytics and data - The better collection of data, combined with greater visibility and control, come together to offer a new level of facility optimisation. By leveraging artificial intelligence, data and analytics, it’s possible to have a single control, always visible, and continually learning system to run a facility. At Xylem, this confluence of technologies and management practices is called BLU-X: a holistic approach to wastewater management to avoid practices such as bypassing by predicting upstream events through past and current data.

  • Improved maintenance - One of the most frequent problems at wastewater facilities are the breakdowns or clogging up pumps and pipes. Several strategies address these issues, including the tracking and monitoring features mentioned above. Modern pumps, such as the Flygt range of ‘grinder’ or ‘chopper’ pumps, help prevent clogs and also reduce maintenance of the equipment. These modern pumps provide sensor data for maintenance and control. They also make the enforcement of maintenance contracts simpler and more effective.

  • New sanitation technologies - In terms of sanitation chemicals, chlorine is still the most popular due to its low cost and ease of use. Yet there are drawbacks of a chlorine-heavy treatment cycle, including the risk of carcinogens and environmentally damaging contamination in the water supply. Systems using ozone and UV sanitation have matured considerably, offering complimentary enhancements to traditional sanitisation processes. These can fit into major treatment facilities, and are also immensely useful for smaller facilities, site cleaning and ad-hoc applications.

The above enhancements don’t need to replace current facilities. But there is room for improvement, and the combination of digital technologies and modern best practices open a world of choice for current and future wastewater treatment facilities. These can be introduced at various levels, says Mistry:

“The best place to start is creating visibility. Put in a few sensors and start collecting the data, then put it through analytics and dashboards to help your decision making. You can focus on a specific part of the facility, using successes there to motivate for other improvements. Ultimately, you’ll realise efficiencies and operational improvements that didn’t even exist not that long ago. This is probably the most exciting time for a treatment facility, because the possibilities are enormous and very flexible, including modular and single-tank processes.”

About Xylem

Xylem (XYL) is a leading global water technology company committed to solving critical water and infrastructure challenges with technological innovation. More than 16,000 diverse employees delivered revenue of $5.25 billion in 2019. Xylem is creating a more sustainable world by enabling its customers to optimize water and resource management and helping communities in more than 150 countries become water secure. www.xylem.com.

Contacts:     

Media
Chetan Mistry
+27 11 966 9311
Chetan.Mistry@Xyleminc.com

Xylem Water Solutions South Africa (Pty) Ltd
3A Spier Street, Plumbago Business Park,
Glen Erasmia, Kempton Park, Gauteng, South Africa
Tel +27 11 966 9300