It looks like you are coming from United States, but the current site you have selected to visit is Oman. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Xylem selected for phosphorus removal at United Utilities site

BioMag® system chosen to help deliver new phosphorus commitments

Xylem has been selected by United Utilities and its design and construction partner, Advance Plus, to supply its BioMag® ballasted clarification system to reduce phosphorus at both the Horwich and Burnley Sewage Treatment Works in Lancashire.

Challenge

Algal blooms and poor river ecosystems are triggered by high levels of phosphorus in the river, which can come from a variety of sources, including agriculture and treated wastewater. To help combat the blooms and restore water bodies to “good” status, the UK Environment Agency’s Water Industry National Environment Programme (WINEP) is imposing low phosphorus limits on many wastewater treatment plants, including Horwich (30,000 population equivalent) and Burnley (147,000 population equivalent). The introduction of the BioMag system will significantly decrease the amount of phosphorus that the works discharges, making this an important step to achieving compliance with the new phosphorus limit of 0.25 mg/l of total phosphorus (T-P).

"By adopting this innovative new technology at both our Burnley and Horwich Wastewater Treatment Works, we will be able to deliver our new phosphorus commitments at a significantly lower whole life cost than a conventional treatment solution."
LISA MANSELL, CHIEF ENGINEER – INNOVATION, FOR UNITED UTILITIES

An innovative solution

The BioMag system uses the addition of magnetite – iron oxide particles – to enhance the existing activated sludge process. As a result, the settlement across the existing final settlement tanks is greatly improved, resulting in significantly better effluent quality. As a result of enhancing the existing activated sludge process, no further treatment is required. For communities that face challenging wastewater characteristics due to industrial discharge or dense populations, the BioMag system is the ideal solution. The BioMag system will help United Utilities reduce both total suspended solids and phosphorus before the treated water discharges into the local rivers. 

‘’For Horwich and Burnley, the new BioMag system will be installed to reach the new phosphorus limit,’’ explains Simon Radford, UK Sales Manager of Xylem’s Wastewater Treatment division. ’’As an alternative to adding a tertiary solids removal step, the BioMag system simply enhances the existing performance of the activated sludge process and allows more treatment capacity to a better quality”.