It looks like you are coming from United States, but the current site you have selected to visit is Oman. Do you want to change site?
The LORENTZ warranty describes that LORENTZ pumps are designed for pumping water for humans and animals. Pumping other liquids is not covered by this warranty.
The water should not contain solids or long fibred particles larger than sand grains.
There are different units for measuring particle concentrations in water. However, there are easy ways to compare the units, e.g. 1g/m3 = 1ppm = 0.0001%.