It looks like you are coming from United States, but the current site you have selected to visit is Qatar. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Case Studies

Case Studies

  • Orange County water district removes PFAS with 30 systems

    In February 2020, the California State Water Resources Control Board announced revised drinking water Response Levels for perfluorooctanoic acid (PFOA) and perfluorooctanesulfonic acid (PFOS) in drinking water. The new Response Levels (RLs) were set at 10 parts per trillion (ppt) for PFOA and 40 ppt for PFOS. The previous RL was 70 ppt for a combined total concentration for the two contaminants.
  • Xylem ensures that potential bacteria is eliminated before water reuse

    Norfolk Southern has a history of nearly two centuries of service that has linked communities and customers to the marketplace of the world. The railway company operates approximately 20,000 miles of rails and serves every major container port in the eastern United States while providing connections to other rail carriers.
  • Xylem partners with COPEG to control screwworm re-infestation

    The Commission for the Eradication and Prevention of Screwworm (COPEG), created by a cooperative agreement between the Republic of Panama and the United States of America, safeguards Panama and the rest of the countries in Central and North America from screwworm re-infestation.
  • Xylem's utrafiltration solution to unpredictable feedwater

    A steel mill located in the Ohio River Valley of the United States had been treating raw river water via a clarifier, gravity filters, multi-media filters, cartridge filtration, and reverse osmosis(RO) to produce demineralized water for the mill rolling lines. In 2014, the mill began experiencing numerous problems with high solids carryover from their aging clarifier to downstream equipment.
  • Fertilizer manufacturer treat organics in rainwater runoff

    Xylem was contacted by a leading US producer of fertilizers and pesticides and consultative services in the field of agricultural technology. Site managers for the company were seeking a solution for treating the rainwater runoff, which was contaminated with pesticides, to keep the contaminants from flowing into local water sources or leaching into groundwater.
  • Industrial wastewater treatment with low profile air strippers

    Industrial process and wastewater can contain volatile organic compounds (VOCS) that can have a negative effect on the production process or downstream wastewater treatment processes. In these instances, it is often necessary to put treatment equipment in place to remove the VOCs.
  • Limiting wastewater cadmium levels

    In August 2010, an electroplating facility in California specializing in aircraft components was issued specialty permit levels for the reduction of cadmium in discharge wastewater. The current permit of 250 ppb was reduced to 70 ppb and the allowed cadmium levels are expected to move lower over the next few years.
  • Microfiltration system eliminates metal generated by manufacturer

    Marathon Norco Aerospace located in Waco, Texas is one of the few manufacturers of rechargeable, nickel cadmium batteries for the aerospace industry. One of the production problems associated with the manufacture of rechargeable, nickel cadmium batteries is the use of a number of heavy metals.
  • Mobile water treatment averts wastewater release

    Piney Point is the site of an inactive fertilizer facility. Following a bankruptcy filing by the parent company in 2001, the site was taken over by the State of Florida to oversee closure. Heavy rainfall and tropical storms in 2001 demanded immediate response to a potential breach of the site's pond dikes and hundreds of millions of gallons of acidic wastewater.
  • Performance under pressure: treating zinc from a retention pond

    The site of a former zinc smelter in the eastern United States, whose soil and groundwater were contaminated after decades of zinc production, posed a significant treatment challenge: the water in the newly created retention ponds had a dissolved zinc level of about 10 ppm, well above discharge limits of <0.47 ppm.
  • Removing zinc from wastewater to meet compliance for automotive part manufacturing

    A Midwest manufacturer of automotive parts was experiencing elevated levels of zinc in the effluent from their existing conventional wastewater treatment system. This wastewater was generated through a multi-stage cleaning and zinc phosphate process which produced elevated levels of both particulate and dissolved zinc in the wastewaters.
  • Cheesemaker captures money-saving biogas with cover system

    Since 1956, Rothenbühler Cheesemakers has been producing delicious cheese using all natural ingredients and 100% Grade-A milk. Formerly known as Middlefield Cheese, the family-owned company is one of the largest Swiss cheese manufacturers in the United States.
  • Cheesemaker saves money and the environment with ADI-BVF® reactor

    Since 1956, Rothenbühler Cheesemakers has been producing delicious cheese using all natural ingredients and 100% Grade-A milk. Formerly known as Middlefield Cheese, the family-owned company is one of the largest Swiss cheese manufacturers in the United States. Its plant in Middlefield, Ohio, USA, produces five Swiss cheese varieties, as well as high-quality whey ingredient products.
  • Confectionery manufacturer eliminates sludge dewatering

    The client makes several types of confectionery products at its facility. Its wastewater was being treated in a dissolved air flotation (DAF) system, followed by a dual-tank sequencing batch reactor (SBR) activated sludge system.
  • Confectionery manufacturer expands its operations with ADI-BVF® reactor

    The confectionery manufacturer, located in Virginia, was faced with having to establish on-site wastewater pretreatment at its facility. A planned expansion and an overloaded publicly owned treatment works (POTW) led local authorities to require wastewater pretreatment in order to meet discharge limits of 250 mg/l for both biochemical oxygen demand (BOD) and total suspended solids (TSS).
  • Confectionery upgrades wastewater treatment system

    An ADI Systems client was equipped with an anaerobic wastewater treatment system that consisted of an equalization tank, three hybrid anaerobic reactors, a degas tower, and a clarifier. This system was not meeting the client’s needs, as it was only removing approximately 60% of the BOD. Sludge settleability and odor issues in the open clarifier also presented a problem.
  • Cover at Pinnacle Foods harnesses energy from anaerobic digestion

    When Pinnacle Foods’ acquired the Wish-Bone® and Western® salad dressing brands, its production plant in St. Elmo, Illinois, USA, would need to expand for additional flow. As part of the wastewater treatment plant expansion, Pinnacle Foods introduced anaerobic digestion technology.
  • Cover keeps plant treatment system operating successfully for 25 years

    The plant is located in an urban setting, surrounded by residences and businesses. Odor from the treatment system is a prime concern for the milk processor. When the milk processor acquired the plant, the biogas collection cover on the wastewater treatment system’s anaerobic digester was nearing the end of its intended service life.
  • Xylem and the City of Tulare celebrate a quarter century of keeping California clean

    The City of Tulare, USA, located in California’s world renowned San Joaquin Valley, has some of the strictest environmental regulations in the nation to protect the Golden State’s water quality. Noncompliance can be costly—up to $10,000 a day. Tulare is committed to complying with wastewater discharge requirements set forth by the California State Department of Water Resources Board.
  • Xylem helps AB Mauri rise above its wastewater challenge

    AB Mauri, a division of Associated British Foods (ABF), is one of the world’s largest producers and distributors of bakery ingredients such as yeast, spices, and bread and cake mixes. AB Mauri’s holistic approach to baking includes a wide range of chemistry and technology applications in addition to its high-quality end products.