It looks like you are coming from United States, but the current site you have selected to visit is Tajikistan. Do you want to change site?

Yes, please! No, keep me on the current site

Performance under pressure: treating zinc from a retention pond

Equipment and media solution enables new owner of a zinc smelter brownfield site to meet remediation requirements and move ahead with development

Challenge

The site of a former zinc smelter in the eastern United States, whose soil and groundwater were contaminated after decades of zinc production, posed a significant treatment challenge: the water in the newly created retention ponds had a dissolved zinc level of about 10 ppm, well above discharge limits of <0.47 ppm.

In order to begin redevelopment, the owner proposed a system to be put into place that could make the water safe for discharge and operate persistently as the ponds refill with rainwater and leach zinc. The construction schedule required that the solution be in place immediately. Xylem was contacted in March 2013 to develop a complicated solution. In addition to a tight deadline, requirements included a solution that was compact, low in capital cost, and as self-sustaining as possible, requiring minimum operator involvement or on-site processing.

Solution

Xylem’s recommendation was a configuration of the Vantage® PTI series multimedia filter and WWIX tanks equipped with SCU™ specialty media. SCU media was designed to remove trace levels of metals such as mercury, lead, cadmium, nickel, zinc, copper, and chromium from complex wastewater to levels not possible with standard ion exchange resins. This class of adsorbents can routinely achieve levels below 1 ppb for most metals.

With proven results that the recommended WWIX configuration could meet zinc limit, volume and timing requirements, the customer approved an installation. This consisted of Xylem’s Vantage Pre-Treatment Industrial (PTI) multimedia filter for 50-100 micron particulate removal, bag filters for 10-micron particulate removal, as well an array of ten IX-48 48-inch diameter vessels equipped with SCU specialty media to remove the zinc to safe discharge levels.

Xylem enabled the developer to meet remediation requirements for zinc contaminated groundwater so they could move ahead with development for the site.

Results

The system was installed in July 2015, meeting the customer’s deadline for remediation. A pumping system draws 350-500 gallons per minute from the retention ponds for treatment, maintaining safe water levels in the ponds as they continue to refill from rain and spring water. Compared to large on-site treatment alternatives, Xylem met the customer’s need for low cost and low profile solution. With remediation needs met, the developer is now free to take the project to the next stage.