It looks like you are coming from United States, but the current site you have selected to visit is Tajikistan. Do you want to change site?

Yes, please! No, keep me on the current site

Anomaly Detection

Get notified if a connected device deviates from the expected behavior, such as decreased pump capacity or inconsistent water level

An anomaly is a deviation from the expected value or trend, or an event that deviates significantly from the normal behavior. The anomaly detection service is enabled automatically when there is an anomaly type that is applicable to the station. The anomalies can be found in the main menu for all your stations, or in the station menu for a specific station. 

Secure Connect shows anomaly notifications from the connected devices. The notifications can be marked as read or unread, but are automatically marked as read after 180 days. 

Anomaly types are specific for the type of station. If any anomaly type is applicable to the station when the station is created, the anomaly detection service is enabled by default. For a station, it is possible to disable the the overall anomaly detection service and the detection of a specific anomaly type. Anomaly types apply to different devices dependent on which data points the devices give. Users are notified of anomalies through in-app notifications.

Types of anomalies Secure Connect will discover

Related FAQs

Many users have had similar questions about Events, Alarms, anomalies and incidents.