-
Golden Flake Eliminates Sewer Surcharges With ADI® MBR System
Golden Flake’s 50 acre (20 hectare) Birmingham, Alabama, USA, corporate headquarters is home to a 350,000 ft2 (32,516 m2) manufacturing facility that processes more than 20 million lb (9 million kg) of snack foods per year. The plant’s production mix can fluctuate, causing its wastewater to have varying strengths and consistencies, with flow rates ranging from 100,000-350,000 gpd (380-1,330 m3/d).
-
Goulds Water Technology dealer goes the extra mile to deliver water to homes outside the reach of municipal water
Chris Hock, owner of North Valley Pump Service, Cave Creek, AZ is a professional residential water systems installer. Chris was approached by a local homebuilder inquiring into the possibility of tapping the municipal water supply contained in a storage tank outside the town of Rio Verde.
-
Leading Texas dairy expands production capacity
Lone Star Dairy is a leading producer of value-added dairy ingredients derived from locally-sourced milk. While Lone Star Dairy was already enjoying the benefits of low-rate anaerobic digestion, production capacity was driving flows and loads beyond the capacity of their existing system. Upgrades were needed to remain compliant to protect the downstream publicly owned treatment works (POTW).
-
Temporary DAF system supports refinery outage
A temporary wastewater treatment system was deployed during a planned outage to support operations while two existing DAF units underwent repair. -
Utility reduces CSO volume by 80%, saving $400 million in CapEx spending using “smart sewer” technology
Predictive monitoring and automated control optimized combined sewer operations, reducing overflow volumes and deferring major capital infrastructure investment.
-
Xylem Lowara contributes to the rebirth of the Molino Stucky
The heart of the heating system features a set of “In-line” centrifugal pumps complete with Hydrovar® frequency converter model FCSH4 150-250/150 – FCS4H 125-200/55; these distribute water to 8 heating subsystems specific to the various buildings in the complex. Each subsystem features a series of multi-speed circulators which independently satisfy the demand of each single building. -
Servicios de Agua Drenaje de Monterrey: Reducing non-revenue water and controlling pressure
Regulate and monitor pressures, supervise flow rates, consumption, and non-revenue water (NRW) in different sectors, and bring together system information from various sources including the SADM’s SCADA.
-
26th Ward WWTP Bypass
The estimated flow through this regulator was 85 MGD, with a combined plant capacity of 170 MGD. Local environmental regulations restricted the use of diesel engines to 175 HP or less, and all engine driven equipment was required to be sound attenuated to 50 decibels at 30 feet.
-
A systems approach to energy and water efficiency in commercial buildings
New building codes continue to raise efficiency standards for new and existing buildings; economic conditions pressure organizations to cut energy costs wherever possible; and new corporate sustainability initiatives require steady efficiency improvements.
-
A temporary pre-treatment solution for a remote coal basin
Xylem built a coal ash disposal solution that met regulatory requirements while controlling labor and fuel costs.
-
-
ADI® MBR chosen by speciality potato processor to treat wastewater
Les Aliments Bari Inc.’s processing plant in Saint-Léonard-d’Aston, Quebec, Canada, needed a new wastewater treatment solution. In the past, wastewater was stored in large tanks on-site that was then applied on local farmland when weather permitted.
-
Advanced analytic solutions used to implement state-wide monitoring program to improve asset reliability and resiliency
Air Selangor is a large water distribution company owned by the Malaysian state of Selangor. The public utility serves a population of 8.4 million residents and manages over 6200 kilometers of trunk mains, ranging from 300mm up to 2200mm, with much of the pipelines located in remote areas of the state.
-
Advancing carbon capture: sensor technology to monitor safely and at scale
Discover how Sentec partnered with a leading CCS operator to identify sensor technologies and integration pathways for safe, scalable CO₂ monitoring, enabling safer long‑term storage, reduced operational complexity, and regulatory‑ready deployment strategies. -
Advancing Sustainability for Gas Utilities with AMI
Thinking about investing in or expanding your advanced metering infrastructure? One of the many benefits - AMI can help support gas utilities in their carbon reduction goals. This infographic explores the value of AMI in reducing truck rolls and supporting sustainability.
-
-
-
-
-
Alberta Utility Averts Potential Catastrophic Holiday Failure with Proactive Pipeline Management Approach
To ensure safe and reliable water service for its customers, EPCOR partnered with Pure Technologies, a Xylem brand to complete a high-resolution condition assessment. The team inspected a 9.4-kilometer (5.8-mi) section of the critical Northside Pipeline for leaks and pipe wall deterioration.
-
ALJARAFESA: Advanced water cycle asset and work order management
Discover how ALJARAFESA modernized water cycle operations with a unified digital platform that connects asset management, maintenance, and leak detection to improve efficiency, responsiveness, and service delivery. -
ApaVital S.A.: Reduction of daily water losses by over 800 m³
ApaVital deploys Xylem Vue to reduce daily water losses by over 800 cubic meters, achieving compliance with EU regulations. -
App Note: Considerations for Sea Cage Aquaculture
The consumer popularity of marine finfish in recent years has led to an increase in the demand for the culture of traditional species and also experimentation with several newer species.
-
App Note: Jag Ski Creates Versatile Platform for Bay Study
Webb’s work with his Jag Ski – named in honor of University of South Alabama’s Jaguars