It looks like you are coming from United States, but the current site you have selected to visit is Kosovo. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

Videos

Videos

  • Video

    Meter Data Analytics

    Xylem Vue’s Meter Data Analytics application optimizes the full potential of utility AMI investments.
  • Video

    Pool Surface Disinfection with Ozone

    From the locker rooms to the pool surface, the PC3 portable ozone cart can disinfect and sanitize any surface that it comes in contact with
  • Video

    Xylem’s Rule LoPro bilge pump

    Xylem’s Rule LoPro bilge pumps are designed for low-clearance boat bilges. The LP900S features electronic automatic sensing and dual water-level modes; the LP900D operates via float or panel switch. Both models include a 180° rotating discharge body and multiple port sizes.
  • Video

    Xylem’s Rule Shower Drain Pump System: Installation, servicing & cleaning improvements

    Xylem’s Rule Shower Drain Pump System model 98B is the next-generation marine shower drain solution from Xylem’s Rule brand, redesigned from the ground up to address the real-world challenges boaters face when installing, servicing, and cleaning shower drain systems in tight spaces. This page provides a full product overview video and written summary comparing the 98B model to its predecessor, the 98A model, so you can understand exactly what changed and why.
  • Video

    SC School Water Fountain Install

    Upgraded water fountains and bottle filling stations now provide 1,000 South Carolina students with safe, lead-free water—made possible by Xylem’s Walk for Water fundraiser and community partners.
  • Video

    Servicing a Jabsco Quiet Flush Marine Toilet

    Step-by-step instructions on how to service a Jabsco Quiet flush marine toilet (37045 and 37245 models) using service kit 90197-0000, including how to take the pump assembly apart and identifying which way the seal goes.
  • Video

    Sewer Management for wastewater

    Xylem Vue's Sewer Management application helps network operators stay ahead of emerging challenges by combining real-time sensor data and intelligent alerts with embedded digital twins for overflow forecasting and evidence-led what-if decision-making across sewer and wastewater networks.
  • Video

    Smarter Water Management in Mining Video

    Smarter water management in mining starts with a holistic view of how your operation uses water from sourcing to dewatering to reuse to everything in between. Whether water is scarce or plentiful at your site, thinking about every step as part of a process versus a standalone function is how Xylem finds ways to integrate your water management to increase productivity, reduce costs and turn water management from an expense to a strategic advantage.

    For over 170 years, Xylem has led the way in water management. We can analyze, customize, engineer, and install a complete solution that will help you focus on your core business, build profitability and solve complex challenges the right way. See what industrial-strength thinking can solve for you.

  • Video

    SonTek ADCP boat and platform options

    SonTek Hydrology Manager for Europe, Lee Pimble, reviews some of the options to consider, from basic boards to the handy remote control and autonomous versions.
  • Video

    Stratmoor Hills Uses Ion Exchange Resin to Mitigate PFAS

    Stratmoor Hills Water & Sanitation Districts (SHWSD) transitioned from seasonal to year-round drinking water treatment, mitigating PFCs including PFOA and PFOS. Currently their treated effluent achieves consistent levels of non-detect for targeted PFAS. This centralized treatment facility is pristine and a source of pride for SHWSD.