It looks like you are coming from United States, but the current site you have selected to visit is Kosovo. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

Setting the daily water amount

The S-Connect App has a function called "Daily amount" that can be activated when needed.

This function allows you to set the maximum limit of water pumped per day in cubic meters (m³) or US Gal (depending on the unit of measure configured).

There is also a function where you need to set a reset time to determine the hour at which the established amount will be reset for the next day.

Therefore, if the set daily amount is reached, the pump will shut off until it reaches the set time to restart again.

How to activate the daily water amount function?

  • Select "Settings"
  • Enable the "Daily Amount" function
  • In the "Set Value" field, enter the maximum amount of water you want to pump in a day.
  • In the "Reset at" field, enter the hour at which you want the "Daily Amount" counter to reset again.

As soon as this option is activated, two bars will appear on the dashboard: the blue bar indicating the amount of water pumped and the green bar indicating the countdown to restart.

 

Further reading

The amount of water pumped in the app is wrong

Reducing the amount of water pumped / Adjusting motor speed