It looks like you are coming from United States, but the current site you have selected to visit is Yemen. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Road show brings Flygt technology to customers

Road show brings Flygt technology to customers

Xylem has developed two mobile showrooms that are now travelling across America to give customers an up-close look at the latest Flygt and Godwin technology for water and wastewater systems. The mobile units will be visiting trade shows, customer locations, distributor-sponsored venues and consultant seminars.

The larger mobile showroom, 24 feet long, has drop-down doors that convert into decks where customers can watch product demonstrations and interactive videos. The decks are also used as training stations, and include high-definition multimedia interfaces.

The informative exhibits include a working display of the Flygt Experior system. The Flygt Experior is built with the innovative Flygt Adaptive N pump, a premium efficient motor and SmartRun controls in a pre-engineered TOP basin. Experior is gaining widespread interest by providing a simple, reliable wastewater pumping solution that delivers energy savings of 50 percent or more.

One of the most popular features of the mobile showroom has been the opportunity to request a free condition audit of a lift station or other Flygt-equipped installation, as part of the TotalCare Program recently announced by Xylem. The mobile showroom also includes an interactive demonstration unit of the Flygt MultiSmart Intelligent Pump Station Manager, along with the Flygt Slimline Propeller Pump and a 4630 Mixer Unit. A Flygt A-C series NS-Custom Pump display provides information about the expansive line of Flygt custom pumping solutions.

Also prominently featured on the front stage is the Godwin Dri-Prime Backup System Pumps (DBS). This unit can be powered by many different fuel types including natural gas and propane. DBS Pumps are designed to be permanently mounted as complete back-up pumping systems to assume continued operation of water and wastewater facilities during power failures or to support bypass flows during repairs or routine maintenance of the station’s existing pumps and controls. The DBS Pumps are more efficient than standby generators by only running when called to pump. This conserves fuel in conditions where refueling may be challenging.

For more information: www.flygtroadshow.com

Showroom for pressure sewerage systems

A smaller, 12-foot long trailer is dedicated to the innovative Flygt pump solutions for pressure sewer applications. This mobile showcase should interest engineers, developers, builders and contractors engaged in residential, multifamily or high-occupancy institutional facilities where pressure sewerage systems are a more efficient and cost-effective solution than excavating deep-trench connectors to collection systems. The display includes a working Compit Pump Station and cutaway display of a Flygt Progressive Cavity (PC) pump.

Also included in the walk-through showcase are the FGC211 control and both pressure bell and 3-point probe level controls. Secondary components include the different size Flygt fiberglass basins with guide-rail assemblies for PC and centrifugal pumps, a counter display of wet-end components on pumps. The exhibit of Flygt solutions also offers a side-by-side comparison with competitive offerings in the industry.

For more information: www.pssroadshow.com

by Simon