It looks like you are coming from United States, but the current site you have selected to visit is Yemen. Do you want to change site?

Yes, please! No, keep me on the current site

How to Calibrate the DEPOLOX® Pool Compact Controller

The DEPOLOX® Pool Compact Controller is applicable for the measurement of chlorine, pH, ORP and temperature.

Chlorine Calibration

During calibration for free chlorine, a zero point calibration and a measured value calibration (DPD1) must be carried out.

Zero Point Calibration

  1. Press the symbol with the horizontal lines
  2. Press the menu Calibration "Cal"
  3. Tap the measurement "Chlorine"
  4. Press the parameter "Zero point"
  5. Close the ball valve on the sample water inlet
  6. Wait until the displayed chlorine value no longer changes
  7. Press the "Calibration" button. An input field opens
  8. Press "Enter" to save the zero point
  9. Open the ball valve on the sample water inlet
  10. After zero point calibration, wait at least 2 minutes

Measuring Value Calibration (DPD)

  1. Open the sample extraction unit (drain) by approximately 1 turn and extract a specimen of the sample water
  2. Determine the content of free chlorine in the sample using a photometer
  3. Press the parameter "DPD"
  4. Press the "Calibration" button. An input field opens
  5. Use the input keys to enter the determined value
  6. Press "Enter" to save the entry

This concludes the calibration of free chlorine.

PH Calibration

  1. Press the symbol with the horizontal lines
  2. Press the menu Calibration "Cal"
  3. Tap the measurement "pH"
  4. Press the parameter "pH 7"
  5. Close the sample water inlet and sample water outlet and briefly open the sample extraction unit (drain) to release the pressure. Close the sample extraction unit (drain) again
  6. Place the beaker into the bottom clip and fill with buffer solution "pH 7.00" or clamp the bag with buffer solution "pH 7.00" into the bottom clip
  7. Unscrew the pH sensor from the cover of the cell body of the flow cell
  8. Dip the pH sensor through the top clip at least 2 cm deep into the buffer solution and move slightly until the indicated pH value remains constant
  9. Press the "Calibration" button. An input field opens
  10. Use the input field to enter the value to be calibrated for the buffer solution
  11. Press "Enter" to save the entry
  12. Remove the buffer solution "pH 7.00" from the bottom clip
  13. Wash the sensor in distilled water to prevent carryover of buffer solution
  14. Press the parameter "pH X"
  15. Place the beaker into the bottom clip and fill it with buffer solution "pH 4.65" or clamp a bag with buffer solution "pH 4.65" into the bottom clip
  16. Dip the pH sensor at least 2 cm deep into the buffer solution and move gently until the indicated pH value remains constant
  17. Press the "Calibration" button. An input field opens
  18. Use the keypad to enter the value to be calibrated
  19. Press "Enter" to save the entry
  20. Remove the pH sensor from the top clip
  21. Screw the pH sensor into the cover of the cell body of the flow cell
  22. Open the sample water inlet and outlet again

This concludes the pH calibration.

ORP Calibration (REDOX)

  1. Press the symbol with the horizontal lines
  2. Press the menu Calibration "Cal"
  3. Select the "ORP" measurement menu
  4. Press the parameter "Cal. value"
  5. Place the beaker into the bottom clip and fill it with calibration solution "478 mV" or clamp a bag with calibration solution "478 mV" into the bottom clip
  6. Close the sample water inlet and sample water outlet and briefly open the sample extraction unit (drain) to release the pressure. Close the sample extraction unit (drain) again
  7. Screw the ORP sensor into the cover of the cell body of the flow cell
  8. Dip the ORP sensor through the top clip at least 2 cm deep into the calibration solution and move it slightly until the indicated pH value remains constant
  9. Press the "Calibration" button. An input field opens
  10. Use the keypad to enter the value to be calibrated
  11. Press "Enter" to save the entry
  12. Remove the ORP sensor from the top clip
  13. Screw the ORP sensor into the cover of the cell body of the flow cell
  14. Open the sample water inlet and outlet again

This concludes the ORP calibration.

Temperature Calibration

  1. Press the symbol with the horizontal lines
  2. Press the menu Calibration "Cal"
  3. Tap the measurement "Temperature"
  4. Press the parameter "Cal. value"
  5. Perform comparative temperature measurement
  6. Use the keypad to enter the value to be calibrated
  7. Press "Enter" to save the entry

This concludes the temperature calibration.

Safety Tip

The above instructions are meant to be a general guideline. Always refer to the owner's manual for your specific system.