-
Bringing pumping efficiency beyond par
England’s Northumbrian Water Ltd (NWL) serves roughly 2.5 million people with water and sewerage services. To better assess its predicted results they conducted a project to measure how much the installation of N-pumps had reduced their costs.
-
-
-
Successful Trials with Flygt Adaptive Mixing Technology
The 4220 mixer comes in 1.5-, 2-, 3-, and 4-horsepower models. A four-horsepower mixer can operate at any lower power level and perform with the same high efficiency as a lower power model.
-
-
-
-
Efficient Handling of Wastewater at a Harbor
One of the ports within the Ports of Stockholm was outfitted with a Flygt pump station for the handling of sewage and grey water. To handle the large amount of waste water without clogging, a Flygt TOP pump station including N-pumps was installed.
-
Enhancing Resilience for London’s Silvertown Tunnel, a major piece of transport infrastructure
Discover how Xylem delivered six pumping stations to prevent flooding in London’s new Silvertown Tunnel, ensuring safe, reliable transport for 25,000 vehicles daily.
-
Mixing It Up in Michigan
Before deciding on the 4320s, Kennedy Industries along with YCUA operations and maintenance personnel performed an extensive energy study of the aeration mixers.
-
Sludge Handling in Perry, Oklahoma
The city needed to discharge sludge at two different rates–one rate for sludge returning to the headworks RAS and another rate for sending material to the sludge box. The system is designed to speed up dewatering biosolids as a replacement to the existing sand drying beds.
-
Pump station retrofit ends stormwater woes in Lyndhurst, NJ
Lyndhurst officials prefer Flygt's submersible-pump solution for its sewer department’s stormwater station.
-
Pumping system with integrated intelligence eliminates chronic clogging and debris buildup in pump station
The city of Sublimity reduced maintenance costs for a problematic wastewater pump station while creating flow capacity for future residential growth. -
Remote monitoring & controls for unmanned reliability
Xylem was tasked with designing a seep collection system to collect water from a low volume seep through the wall of a decommissioned fly ash pond. The sump was located in an active river floodplain that flooded with as little as 1-2 inches of rain, so the customer needed an automatic shutdown when the river covered the sump.
-
Remote Pumping Solution helps Mine Operators Reach New Depths in Harsh Environment
A customer in Perú needed to drain water as its large open-pit mine operation reached as deep as 1,200 ft (365 m) below the surface. The discovery of more copper in the mine, and an expected excess of water during rainy summer months also prompted the company to act. They sought a remote solution for monitoring and controlling their pumping system, particularly as routing electrical power became more difficult the deeper they dug....
-
-
-
-
-
-
-
Xylem’s Holistic Solution of Mixers and Pumps Supports Efficient Mine Slime Transport – From Sump to Surface Disposal
One customer, operating a hard rock nickel mine in Ontario, needed an efficient and reliable solution to transport its mine slime from an underground sump back to the surface while ensuring continuity in production and minimizing downtime.
-
-