-
Intelligent pumping supports United Utilities' CSO programme
Xylem and United Utilities collaborated to transition 330 sites to just three standardized pump types, simplifying maintenance and cutting inventory by 85%. This smart network rollout also slashes reactive service calls by over 90% while lowering energy consumption by up to 40%. -
Rented pump system supports major Scottish Water refurbishment
A temporary pumping system enabled improvements to be completed at a major Scottish Water pumping station, ensuring uninterrupted operation throughout a 10-month project -
Temporary bypass solution maintains treatment operations
Discover how Xylem maintained uninterrupted wastewater treatment during critical screw pump maintenance with a compact bypass pumping system, balanced flow distribution, resilient backup power and 24/7 remote monitoring. -
Managing complex temporary bypass flows
Discover how Xylem delivered a resilient temporary bypass pumping solution capable of managing peak flows of up to 500 l/s, maintaining uninterrupted wastewater services and ensuring operational resilience during critical network infrastructure works. -
Beating the blockages at Rochfort Manor
How Flygt Concertor eliminated pump blockages, improved reliability, and delivered over 70% energy savings for Irish Water. -
Zero unplanned failures since 2013
Planned Maintenance Agreement delivers budget predictability and zero unplanned failures for Municipality of Scott -
Pumping system with integrated intelligence eliminates chronic clogging and debris buildup in pump station
The city of Sublimity reduced maintenance costs for a problematic wastewater pump station while creating flow capacity for future residential growth. -
Sörbyvägen Sewage Pumping Station
In conjunction with the expansion of a new pedestrian and cycle path along Route 160, specifically the section between Sörbyvägen and Myggenäs, new water and sewage pipelines were installed. As a vital component of this project, a new sewage pumping station was established to ensure reliable and long-term wastewater management for the area. -
Intake pumping stations P1 and P2 in Kristianstad
As part of Kristianstad Municipality’s investment in a new wastewater treatment plant, construction of two new intake pumping stations – P1 and P2 – began in 2022. The stations play a central role in the facility and are designed to pump wastewater from the trunk sewer network to the new treatment plant. The project was carried out between March 2022 and November 2024. -
Xylem as turnkey contractor for the new pumping stations in Bromstensstaden
Urban development in Bromstensstaden required new, reliable wastewater pumping stations to meet increased demands on the water and wastewater system. -
Xylem as turnkey contractor for a new pumping station solution in Kristvallabrunn
Xylem delivered a turnkey pumping solution in Kristvallabrunn, including a new pumping station and booster station for reliable, energy-efficient wastewater transfer. -
Le pompe Xylem forniscono una soluzione completa per la mitilicoltura olandese
La coltivazione di cozze e ostriche avviene nell’Oosterschelde, un’area protetta di circa 37.000 ettari nel Mare del Nord. In quanto parco nazionale più grande dei Paesi Bassi, l’Oosterschelde è un ecosistema cruciale e un punto di riferimento per la pesca sostenibile di mitili, ostriche e crostacei.
-
Pump Station in Krokom – Unique PE Construction
Xylem delivered a turnkey solution for one of Sweden’s first pump stations featuring a fully integrated PE construction in Krokom. -
Thames Water and Xylem set new standard for pump upgrades at scale
A Xylem and Thames Water partnership represents a shift in how water companies can manage inherited infrastructure. -
-
Welsh Water scales up Xylem’s Flygt Concertor for smarter wastewater management
Dŵr Cymru Welsh Water is scaling up its deployment of Flygt Concertor intelligent pumping systems to improve wastewater network resilience, reduce energy consumption, and support its environmental goals. -
Maximizing biogas production through effective mixing technology and active seal protection
Learn more about maximizing biogas production through effective mixing technology and active seal protection. Read our case study with our customer Nesemeier now →
-
Sustainability success for Dairygold: mixers deliver biogas system results that matter
Flygt mixers deliver sustainable success for Dairygold at the heart of the world's largest ADI-BVF® fermenter. Read the case study →
-
Enhancing resilience for London’s Silvertown Tunnel, a major piece of transport infrastructure
Discover how Xylem delivered six pumping stations to prevent flooding in London’s new Silvertown Tunnel, ensuring safe, reliable transport for 25,000 vehicles daily.
-
Trial of Flygt adaptive mixers shows energy and cost saving in New Plymouth, New Zealand
Xylem collaborated with the New Plymouth District Council to trial the innovative Flygt Adaptive technology, replacing two existing mixers in the anoxic zone of bioreactors.
-
Flygt Concertor wastewater pumping system delivers eight years of high efficiency and clog resilience at Heathrow Airport, while halving station energy consumption.
In November 2015, Heathrow Airport’s water services department installed and trialled Xylem’s new state-of-the-art Flygt Concertor intelligent wastewater pumping system, with the intent to solve chronic clogging issues at one of the airport’s more challenging wastewater pumping stations.
-
Pump replacement project at Gloucester Docks keeps Bristol’s water supply flowing
The four existing column pumps at Gloucester Docks - which are vital for managing water levels in the canal and keeping Bristol’s water supply running - were reaching the end of their working life and needed replacement.
-
Flygt Concertor eradicates wastewater pump blockages for Yorkshire Water
Yorkshire Water’s Dynamic Maintenance Team identified that they required an easily deployable solution that delivered tangible benefits across the network.
-
Flygt hydro turbines prove to be smart solution for small-scale hydroelectric power project
Even in coal-dominated Kentucky, renewable energy is getting more attention as federal and state tax incentives add up, and the federal government moves closer to capping carbon dioxide emissions and making coal power more expensive.