It looks like you are coming from United States, but the current site you have selected to visit is South Korea. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Call Lists

Send alarm notifications to a defined call list through text messages, emails, or inside the app

The call list is a list of users that are notified when there is an alarm. The users are notified in order of priority and with a time delay between each notified user. The priority order and time delay are configured in the application. Users receive alarm notifications through SMS or email. If a user acknowledges the alarm, then the next user in the call list does not receive a notification. Users can set a weekly schedule to specify which days and times they receive notifications.Multiple stations can use the same call list.

Read More

Related FAQs

Many users have had similar questions about Events, Alarms, anomalies and incidents.