It looks like you are coming from United States, but the current site you have selected to visit is South Korea. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

Function and use of tank full switch

With a float switch, the pump works autonomously, saving you time and effort.

The tank full switch is a useful accessory to use with tanks. A float switch detects the level of water in a tank or container.

It floats on top of the water surface and functions as a mechanical switch as the water level goes up or down.

When the tank is full, the accessory sends a signal to the controller to turn the pump off. When the tank is empty, the switch sends a signal to the controller to restart the pump and fill the tank.

Connection to the controller

Connect the tank full switch accessory to the controller input as shown in the following video and place the accesory in the tank.

Activation

The tank full switch accesory can be activated in two ways:

  • Using the S-Connect application (with a Smartphone or tablet) and
  • without using the S-Connect app, in case you do not have a Smartphone at hand.

To activate the tank full switch via the app using a Smartphone, refer to the article below for more information:

Activate the tank full switch using the App

Managing sensor inputs and accessories with the S-Connect app

To activate the tank full switch accessory without using the S-Connect app, see the link below:

Activate the tank full switch without using the App

Activation of accessories without the S-Connect application