Documents
-
Combined Sewer and Stormwater Systems
Handle varying storm and sanitary sewer loads A combined sewer system uses the same infrastructure to handle both wastewater and stormwater. Managing highly...
-
Natural Gas Tapping Solutions
Our tapping sleeves are quick and easy to install with simple hand tools. No special equipment or caulking or welding is required for installation. The process...
-
Advanced Metering Infrastructure (AMI)
Create More Powerful Connections with Smarter Advanced Metering Infrastructure We see it everywhere. Connectedness is the norm. And keeping pace with it...
-
San Diego plant cuts THM levels in half
The 34 MGD Otay Water Treatment Plant in San Diego, California serves a population of approx. 200,000. The plant receives raw water from two sources - imported water from the Colorado River and runoff from three local reservoirs.
-
Sazerac Northwest Ordinance Distilling (NOD) plant upgrades to sustainable anaerobic membrane bioreactor (AnMBR) system
The cost of hauling wastewater caused Sazerac Distilling to upgrade its wastewater treatment system to a sustainable anaerobic membrane bioreactor (AnMBR) system by Xylem. -
SCV Water Agency selects Xylem vessels & media for PFAS removal
Santa Clarita is located about 35 miles north of Los Angeles. The Santa Clarita Valley Water Agency (SCV Water) services nearly 74,000 customers and obtains about 50% of its drinking water through local groundwater aquifers. Positioned behind the William S. Hart community baseball and softball fields three two-vessel systems have been installed to remove PFAS from drinking water.
-
Secure in-field firmware updates to support more resilient connected products
EU Cyber Resilience Act: Manufacturers must report vulnerabilities from Sept 2026, with full compliance required by Dec 2027 -
Temporary DAF system supports refinery outage
A temporary wastewater treatment system was deployed during a planned outage to support operations while two existing DAF units underwent repair. -
Soil and groundwater remediation
Soil and groundwater remediation projects often call for treatment of groundwater, soil vapor extraction condensate, soil vapor and other liquid and vapor streams for removal of volatile and semi volatile organic compounds. Xylem's Carbonair has provided thousands of STAT Low Profile Air Strippers, liquid phase and vapor phase carbon vessels for remediation systems over our 30 plus years in business.
-
Southern California water utility consults Xylem for disinfection of potable water
Located in Southern California, this water utility uses wells to store water. These same wells are also used for fire protection. which is especially critical during the summer months. The supply covers about 10,000 customer connections with chloraminated water for residual disinfection, with chlorine and ammonia boosting in various locations.
-
Specification Tips to Maximize Heat Transfer: Shell and Tube
Heat exchangers are widely used in various industries including chemical, oil & gas, power generation, food & beverage, HVAC & refrigeration, pulp & paper to name a few, and are expecting strong growth over the coming years driven in part by a rising focus on environmental impact and improving efficiency standards.
-
-
Stadtwerke Trier: AI-aided energy optimization for daily energy balancing
Xylem Vue helped Stadtwerke Trier optimize renewable energy use in its drinking water network, achieving 90% self-consumption. -
Sugar company finds sweet solution for odor control
The sugar company produces approximately 4,500,000 cwt. of sugar per year, resulting in high-strength wastewater that creates odors, especially during the company’s peak season in the spring and summer. The company was using a series of basins, such as ponds and ditches, to cool, equalize, settle, and digest the organic wastewater.
-
Taron™ activated sludge filter delivers needed capacity to meet discharge limits
A food processing company’s wastewater treatment plant was struggling to meet local discharge limits and faced a hard deadline for compliance from the local authority. The problem centered on excessive solids in the effluent. To ease the hydraulic load on the existing concrete secondary clarifier and reduce total suspended solids (TSS), Xylem installed a Taron activated sludge filter.
-
Tarragona Water Consortium: implementation of an advanced data management solution
CAT implemented the Xylem Vue platform and its Smart Water Engine to solve this problem and boost water and energy efficiency. The Unified Network Management application was implemented to provide a single control center for CAT’s drinking water treatment assets, regardless of their geographical location.
-
Temporary pumping ensures continuous service during asset replacement
After an unexpected wastewater pump failure, Xylem rapidly installed a temporary NC200 Electric unit integrated with the site’s existing pipework, power and controls to maintain uninterrupted operation during the replacement lead time. Variable speed control and 24/7 Secure Connect monitoring ensured efficient, reliable performance throughout the extended hire period, even when a second pump failed. -
-
-
Intelligent wastewater pumping eliminates clogging and cuts energy use at Heathrow Airport
Flygt Concertor was trialed at Heathrow Airport to solve chronic clogging and delivered clog-free pumping while cutting energy use by 53%.
-
-
Town of Creston Pretreats Brewery Wastewater with ADI-BVF® Reactor
Creston’s wastewater treatment facility treats both domestic and industrial effluent. The Columbia Brewery, which feeds its wastewater to the town, underwent major expansions that significantly increased its wastewater flows. Creston was not equipped to treat the volume of wastewater generated by the brewery. Town officials were eager to solve the problem, especially since the brewery was Creston’s largest employer.
-
Turnkey solution eliminates chain and scraper downtime in Grass Valley, CA
The Grass Valley Wastewater Treatment Plant provides service for a population of approximately 12,000 people. Situated in California’s Gold Country, the area has some unique challenges that include mine drainage and heavy flows during the winter storm season in the scenic Sierra Nevada foothills. On average, the City discharges 2.1 million gallons per day of treated wastewater effluent to Wolf Creek, a tributary of the Bear River.
-
Updating London’s drinking water network
A UK water supply company serves a population of approximately 675,000 consisting of homes and businesses in Surrey, Sussex and Kent and is a key part of London’s drinking water network. The largest works in Kent, which takes raw water from a reservoir that is recharged in winter by abstraction from the River Eden. The original works capacity was 35Ml/d and it is currently undergoing a phased uprate.