-
Severn Trent Water: digital twin to optimise energy and emissions in WWTPs
The implementation of a digital twin at the Strongford treatment works has enabled Severn Trent Water to visualise plant performance in near-real time. -
-
Simplot Partners with Xylem on Wastewater Treatment Projects
The J.R. Simplot Company, commonly referred to as Simplot, is one of the largest privately held food and agribusiness companies. The company is headquartered in Boise, Idaho, USA, but it has operations around the globe, including Portage la Prairie, Manitoba, Canada, and Caldwell, Idaho, USA.
-
Smith-Blair Bell Pack Stops Leaking Sewer Force Main in Miami
The sewer force main was not just leaking into the streets but into the Intercoastal Waterways along the coast of Florida. Smith-Blair engineers developed the solution, sent drawings to the customer, got the drawings approved and then had fabrications team come in specifically to work on the 48 inch bell pack all night.
-
Smith-Blair Dismantling Joint Used In The Panama Canal
The dismantling fitting will allow for easy removal and re-installation of the butterfly valve when valve maintenance is required. These fittings are part of the new Panamanian subway system pipeline relocation project that involves several thousand feet of pipeline.
-
-
Sörbyvägen Sewage Pumping Station
In conjunction with the expansion of a new pedestrian and cycle path along Route 160, specifically the section between Sörbyvägen and Myggenäs, new water and sewage pipelines were installed. As a vital component of this project, a new sewage pumping station was established to ensure reliable and long-term wastewater management for the area. -
Spain: Digital transformation of utility processes and infrastructure
To expand digital transformation initiatives beyond the city of Valencia, and effectively manage up to 400 different services across a widely dispersed geographical area. Due to the nature of the project and the stakeholders involved, Global Omnium needed to integrate the systems, sensors, and communication protocols which were already installed across the various infrastructures it managed.
-
Special Pool Management Systems for Saltwater Pool
The Obermain Therme in Bad Staffelstein invites you to relax : with around 3,000 m2 of water surface, and more than 26 indoor and outdoor pools in the swimming pool and sauna area , there is a wide variety to choose from. The operators invest continuously, modernize and expand to keep the spa attractive and to offer their guests an enjoyable visit.
-
Specification Tips to Maximize Heat Transfer
Heat exchangers are widely used in various industries including chemical, oil & gas, power generation, food & beverage, HVAC & refrigeration, pulp & paper to name a few, and are expecting strong growth over the coming years driven in part by a rising focus on environmental impact and improving efficiency standards.
-
Spoetzl Brewery Treats Wastewater and Taps into Green Energy
Spoetzl Brewery’s white brick Alamo-style plant in Shiner, Texas, USA, produces many year-round and seasonal brews—including Spoetzl’s flagship beer, Shiner Bock. The brewery needed a reliable treatment solution that would effectively handle brewery wastewater so that it complied with pretreatment effluent regulations.
-
Stadtentwässerung Celle: Wastewater treatment plant process optimization through artificial neural networks
Celle cuts energy consumption by 22% and chemical use by 56% using Xylem Vue WWTP optimization technology, saving tens of thousands of euros annually. -
State of the art water treatment technology for a German outdoor pool in Bernsbach
The operators wanted to use non-hazardous table salt with electrolysis for disinfection. They were also looking for a filter technology that generates low wastewater costs and can be installed in a space-saving manner.
-
-
Stone Countertop Company Reduces Dewatering Costs
Stone countertop company, Surface Technology, Inc. of Elkridge, Maryland, knew they needed a larger filter press to improve the efficiency of the company's production system and reduce costs. What they didn't know was how the new press was going to improve their whole system.
-
-
Submersible pumps in concrete pump station, pumping effluent
CV services believed they may have an application that our new Concertor pumps would be ideally suited to help overcome some of the issues they had been experiencing with blockages and constant ragging at one of BAC’s pump stations.
-
Sustainable Cleaning Solution from Moosfrei® Taps into Xylem Technology to Reach New Heights
While visual aesthetics might not be a top priority for home or business owners, if left untreated these colonies can infiltrate the very structure of the building facade. This can cause consequential damage to the building, leading to a substantial loss in property value over time.
-
Tacoma Public Utilities Enhances Customer Experience with Xylem Digital Solutions
Tacoma Public Utilities (TPU), the city’s largest government department, is making it their goal to provide customers with greater control, choice, and convenience showcasing their commitment to enhancing the customer experience for more than 300,000 residents throughout the service area that put their trust in them.
-
Taron™ Activated Sludge Filter Provides Effective Total Suspended Solids (TSS) Reduction
For Pennsylvania’s Western Butler County Authority (WBCA), peak flow events due to inflow and infiltration (I&I) have gone hand-in-hand with aging sewage system and treatment plant infrastructure.
-
Temporary fire protection systems keeps long-term care hospital facility online
Retrofitting or upgrading the fire protection system of an existing facility is not uncommon, necessitating a temporary fire protection solution that integrates with the existing pumping system to ensure continuity and compliance.
-
-
-