Het lijkt erop dat u van United States komt, maar de huidige website die u wilt bezoeken is Netherlands. Wilt u van website wisselen?

Ja, graag. Nee. Ik wil op de huidige website blijven.

Hoog contrast modus inschakelen

The revised Urban Wastewater Treatment Directive: Why it’s time to act

The revised Urban Wastewater Treatment Directive (UWWTD) is set to bring about some of the biggest changes to wastewater regulation in more than 30 years, with increasingly stringent requirements introduced across Western Europe over the coming decade. While many of the implementation deadlines may seem far ahead, early preparation is essential for future compliance, not to mention vital operational benefits. Here, Andrea Maggio, Global Product Manager, Process Intensification at Xylem, explains how plants can improve treatment performance, increase resilience, and unlock long-term operational benefits.

From legislation to implementation

The revised Urban Wastewater Treatment Directive (UWWTD) updates the European Union's framework for collecting and treating urban wastewater, introducing more ambitious environmental standards to improve our water sources. The new legislation includes stricter requirements around nutrient removal, energy efficiency and, for some treatment plants, the removal of micropollutants, with implementation phased in over the coming years.

Now the revised UWWTD is in the national transposition phase, the focus is shifting from legislation to implementation. EU Member States have until 31 July 2027 to transpose the Directive into national law, giving utilities a crucial window to understand future obligations, develop investment strategies and begin preparing for the operational changes ahead. 

With some obligations not applying until the 2030s and beyond, it's understandable to think there is plenty of time. But that's exactly why now is the right time to start planning.

The most successful wastewater treatment projects are never rushed. They are the result of careful planning, robust engineering, phased investment, and a clear understanding of future requirements. Waiting until compliance deadlines begin to loom could leave plants facing higher costs, limited contractor availability and unnecessary pressure to deliver infrastructure upgrades within compressed timescales.

Stronger nutrient removal requirements

One of the most significant operational impacts of the revised UWWTD is the increased focus on nutrient removal. It strengthens Europe's ambition to reduce the impact of excess nitrogen and phosphorus discharged into rivers, lakes, and coastal waters. While the exact requirements will depend on factors such as plant size and the sensitivity of receiving waters, many operators are likely to see tighter discharge consents over time.

For some treatment plants, existing biological nutrient removal processes may require optimisation. Others may need significant investment in additional treatment capacity, enhanced biological processes, tertiary filtration, or new process technologies capable of consistently achieving lower nutrient concentrations. These are all upgrades that take time to plan and implement.

Compliance is only part of the story

The revised Directive isn't simply about meeting future legislation. Early investment can deliver benefits long before new regulations become mandatory. It presents an opportunity to improve treatment performance, increase resilience and prepare plants for the challenges they are already beginning to face. 

Many wastewater treatment plants are already experiencing increasing loads as populations grow. Climate change is also placing additional strain on treatment infrastructure through more frequent storm events and variable flows.

Upgrading treatment processes to improve nutrient removal can help address these existing challenges, including increasing treatment capacity, improving effluent quality, increasing water reuse and lowering energy consumption, while simultaneously preparing plants for future regulatory obligations. 

The CoMag® system is a great example of this. This leading technology for phosphorus removal uses magnetite to enhance the clarification process, settling chemical floc up to 30 times faster than conventional clarification, enabling plants to increase tertiary clarifier performance. 

Time for action

Plants that start assessing their assets, evaluating treatment technologies, and developing investment strategies today will be better positioned for compliance with the revised UWWTD. Not only this, but these plants will also benefit from vital operational and environmental gains in the short term. Let’s not look at compliance with the revised UWWTD as the end goal, let’s look at it as a catalyst for modernising treatment infrastructure to improve long-term operational performance and build a more sustainable water infrastructure for the future. It’s time for action.