Het lijkt erop dat u van United States komt, maar de huidige website die u wilt bezoeken is Netherlands. Wilt u van website wisselen?

Ja, graag. Nee. Ik wil op de huidige website blijven.

Hoog contrast modus inschakelen

Installing the pump in a well

Follow these steps to install the S1–200 in a well.

  1. Make sure the controller is turned off and all cables are connected
  2. Make sure the hose is connected tightly with the hose clamp
  3. Attach a safety rope to the pump (see video below)
  4. Slowly lower the pump into the well
  5. Attach the rope to a pole or similar robust structure next to the well

Further reading

Connecting a hose to your pump