Resultados da pesquisa
-
-
-
Cover helps community control odors from wastewater treatment
When the affluent, new home development was being established, odor control was top of mind. The wastewater treatment plant was in close proximity to the new development, which includes 900 acres (364 hectares) of preserved open space, including 24 miles (38 kms) of trails, 10 neighborhood parks, a community pool and water park, as well as outdoor sport courts.
-
Cover System Helps Vallejo Sanitation District Streamline Plant Operations
The Vallejo Sanitation and Flood Control District is an independent special district created by the State of California to collect and treat wastewater and protect the Vallejo community from flooding. Since 1952, the district has protected public health and the San Francisco Bay Area by treating wastewater generated by the more than 115,000 residents of Vallejo and surrounding area.
-
Dairy Plant Captures Biogas from Anaerobic Digestion
Laticínios Bela Vista expanded their plant in Bela Vista de Goiás and evaluated wastewater treatment options that would meet the company’s commitment to sustainable growth and protection of the environment. Laticínios Bela Vista selected an anaerobic digestion treatment system proven to treat dairy wastewater.
-
Data Center Reduces Energy Usage and Chemical Dosing
A global hyperscale data center customer was looking to operate their cooling water system without continuous chemical dosing. Evoqua worked closely with the customer‘s engineering team to find the solution that would best fit their needs. Ultimately, a combination of media filtration and ultraviolet (UV) was selected and installed.
-
-
-
-
Delivering cost-effective process monitoring for the welding industry
Discover how Sentec engineered a compact, non-intrusive smart connector to digitally transform welding operations. From non-contact wire speed sensing to seamless Bluetooth integration, this case study highlights a scalable solution built for regulation, reliability and industry-wide adoption. -
-
-
Eau d’Azur: France’s first smart water network cuts losses and strengthens drought resilience
The Metropolis of Nice is implementing a hypervision platform, based on Xylem Vue technology, to increase efficiency, sustainability, and resilience by providing a real-time view of the network. -
-
Efficiency Gained Through Automated Aeration Control with a Pulse
For many years, maintaining efficient aeration control was a challenge for the 24 MGD Muncie, Indiana, Water Pollution Control Facility (WPCF). A manually operated system combined with severe mixing-limited conditions resulted in over-aeration and wasted energy. The plant alleviated this problem with automated control and Pulsed Aeration, allowing it to satisfy the needs of the bacteria and mix basin contents while expending less energy.
-
Efficient Handling of Wastewater at a Harbor
One of the ports within the Ports of Stockholm was outfitted with a Flygt pump station for the handling of sewage and grey water. To handle the large amount of waste water without clogging, a Flygt TOP pump station including N-pumps was installed.
-
Bremen's Future District: Sustainable Energy from the River
The investor set out to realize a sustainable and innovative concept that meets the demands of a contemporary urban quarter.
-
Electric Generating Station Maximizes Plant Efficiency
Xcel Energy is a leading provider of electricity and natural gas to customers in the Midwestern US. As part of their expansion plans for the Comanche Station, a coal-fired electric generating station located in Pueblo, CO, Xcel Energy contacted Evoqua Water Technologies to explore cost effective solutions for their water treatment needs.
-
EMALCSA: implementation of a digital twin to support decision-making in water supply network operations
The Empresa Municipal de Aguas de La Coruña (EMALCSA) manages the water cycle in the city of A Coruña and seven neighboring municipalities, serving a total population of 400,000. The utility collects, treats and distributes over 36 million cubic meters of drinking water to 138,000 customers each year, via a network of over 560 kilometers, 26 storage tanks and six pumping stations. -
EMASA: improving water efficiency through smart water balance analysis
EMASA (Empresa Municipal Aguas de Málaga S.A.) is the Malaga City Council’s public utility which has been in charge of managing the entire urban water cycle since 1987. The company serves more than 600,000 residents and supplies approximately 42 hm³ of drinking water. The system operates at a flow rate of up to 2 m³/s, ensuring urban water supply through an extensive pipeline network of around 2,000 km, divided into approximately 240 DMAs (District Metered Areas) and equipped with over 240,000 meters, 170,000 of which are smart devices. -
EMASESA: implementation of a digital twin to optimize decision-making in drinking water and wastewater management
Implementation of the Xylem Vue platform to optimize management, anticipate events, and improve the efficiency, resilience, and sustainability of the water cycle in Seville. -
-
-
Emergency sewer system repair
40-year-old carbon steel pipe with catastrophic failure repaired in hazardous wet well conditions. Smith-Blair 675 restored system integrity with zero downtime.