It looks like you are coming from United States, but the current site you have selected to visit is Angola. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

Setting a timer for the pump

How to set a timer for the pump

To set a timer, go to "Settings".

Activate the "Timer" function and select the type of timer needed. You can choose between "Clock timer" and "Interval timer".

  • "Clock timer" will run the pump only in the time period chosen
  • "Interval timer" will run the pump for the specified time and then pause for a specified time. This process repeats.

 

Further Reading

Downloading the S-Connect app