Resultados da pesquisa
-
Do Not Sell Or Share My Personal Information
Our Privacy Notice describes the circumstances in which we may share your information with third parties and explains that certain companies may place tracking...
-
-
-
Bell & Gossett Selection, Sizing & CAD Tools
General Selection Tools: ESP-PLUS for B&G Centrifugal Pumps, Booster Pumps, Pump Accessories, and Air Separator ESP-PARTS for replacement parts selection...
-
Building Information Modelling - The digital revolution of the construction business
BIM is changing the global construction business across water utilities, industry and building services markets. BIM is also improving the way parties within...
-
The S-Connect app shows motor cable error
If your S-Connect app shows an error with the motor cable, there are several things to check. Please make sure your system is turned off before following these...
-
The amount of water pumped in the app is wrong
The controller calculates water flow based on the selected pump end. When the app first connects to a pump, it forces you to select a pump end. If the pump end...
-
Opening the controller
The controller cannot be opened and attempting to do so could result in bodily harm, while also destroying the controller.
-
Checking the voltage of the pump system
The maximum input voltage of the S1-200 controller is 55 V DC. The open circuit voltage (VOC) of your PV modules must not exceed the maximum input voltage of...
-
Setting the correct pump end type in the app
It is important to select the correct pump end for accurate flow calculation. If the wrong pump end is selected, then the data shown in the S-Connect app might...
-
Exporting pump data in the S-Connect app
Your pump system stores data about solar power, water flow, motor speed, errors and many other things. The data can be accessed in the app while connected to...
-
Reducing the amount of water pumped / Adjusting motor speed
If the water flow is too high for your application, there is an easy way to limit the flow with the S-Connect app. To lower the water flow you simply reduce...
-
Using the S-Connect app with your pump system
LORENTZ S-Connect turns any Android Smartphone or tablet into a management and configuration tool for S-Line LORENTZ pumps. You can easily configure your pump...
-
Checking how much water has been pumped
You can easily check the amount of water pumped in the dashboard of the S-Connect app. Open the app Connect to the pump controller via Bluetooth® Check the...
-
Meaning of LED sequences
The LED sequences on your controller give you information about your pump system. In the video below you find the sequences and their corresponding icons in...
-
How to switch on the S1-200 pump system
The S1-200 ON / OFF switch is located in the top right next to the LEDs. To switch on the system switch to on ( 1 ). The LED will go from flashing green...
-
Using the pump in a horizontal position
The S1-200 can be used in horizontal position as long as it is protected from dirt or mud. Pumping water with higher particle concentrations than indicated...
-
Downloading the S-Connect app
Download the Xylem S-Connect app for use with your S1 system. Xylem S-Connect is available for Android or IOS devices. Xylem S-Connect in Google PlayStore...
-
Controller waterproof/weatherproof rating
The S1-200 controller is built robustly. However, to ensure your equipment lasts as long as possible, install it in a place where it is protected from the...
-
Connecting cable extensions for motor and accessories cables
Motor and accessory cable extensions are available for purchase. They provide an easy plug and play solution for extending cable length. Because of power...
-
Connecting a hose to your pump
The S1-200 pump is designed to be used with a 25 mm (1.0 in) hose. Please refer to this video to learn how to attach a hose to your pump: Further reading Hose...
-
Activation of accessories without the S-Connect application
Activation of dry run protection accessory without S-Connect App In case you do not have a smartphone at hand and wish to activate the dry-running protection...
-
Mounting the controller
There are a few things to keep in mind when mounting the controller: it should not be in sun a shaded place is best it should be protected from rain if...
-
Function and use of tank full switch
With a float switch, the pump works autonomously, saving you time and effort. The tank full switch is a useful accessory to use with tanks. A float switch...