Documents
-
-
Inclusion & Belonging
Xylem is an Equal Opportunity Employer. Employment decisions are made without regard to race, color, religion, national or ethnic origin, sex, sexual...
-
Students & Graduates
Xylem innovates and collaborates with utilities, industrial manufacturers, buildings operators, and communities, to protect and optimize water. Using global...
-
-
Xylem Career Opportunities
Xylem is an Equal Opportunity Employer. Employment decisions are made without regard to race, color, religion, national or ethnic origin, sex, sexual...
-
Webinar
From vibration symptoms to engineering solutions
Pump vibration problems cannot be resolved reliably by looking at vibration magnitude alone. Engineers must connect field symptoms with excitation sources, natural frequencies, installation conditions, and the dynamic response of the complete pumping system. -
Equalization, channels and other process tanks
Equalization tanks, channels, and other process tanks are the backbone of a wastewater treatment plant. -
Blog Page
How incremental digitalization empowers wastewater teams
The article explains how wastewater utilities can adopt digital tools incrementally while strengthening cybersecurity. -
Blog Page
Mimizan deploys the Xylem Vue platform to optimize its wastewater network management
As wastewater utilities face stricter regulatory requirements, while also needing to optimize investments, Mimizan is taking a major step forward in the digital transformation of its service. -
-
Spain: Digital transformation of utility processes and infrastructure
To expand digital transformation initiatives beyond the city of Valencia, and effectively manage up to 400 different services across a widely dispersed geographical area. Due to the nature of the project and the stakeholders involved, Global Omnium needed to integrate the systems, sensors, and communication protocols which were already installed across the various infrastructures it managed.
-
Servicios de Agua Drenaje de Monterrey: Reducing non-revenue water and controlling pressure
Regulate and monitor pressures, supervise flow rates, consumption, and non-revenue water (NRW) in different sectors, and bring together system information from various sources including the SADM’s SCADA.
-
Advanced analytic solutions used to implement state-wide monitoring program to improve asset reliability and resiliency
Air Selangor is a large water distribution company owned by the Malaysian state of Selangor. The public utility serves a population of 8.4 million residents and manages over 6200 kilometers of trunk mains, ranging from 300mm up to 2200mm, with much of the pipelines located in remote areas of the state.
-
Real-time decision support helps cut combined sewer overflow volume by 100 million gallons and reduces capital needed for regulatory compliance
Evansville is located on the north bank of the Ohio River in southwest Indiana. The City’s sewer system, parts of which are more than 100 years old, serves a population of 163,000, with combined sewers making up almost 40 percent of the total sewer area.
-
Wastewater Treatment in Eunice, LA: Retrofit Restores Compliance and Cuts Energy Costs
The new products cut energy costs in half as compared to the 5 previous floating mixers.
-
UV Systems Supplementing Membranes: Drinking water disinfection in Barcelona
Most of the drinking water of the city of Barcelona is drawn from the river Llobregat, the water of which is brackish with differing parameters. The turbidity of the water varies due to sea level and amount of precipitation in the mountains.
-
Brabant Water: end-to-end advanced water supply digitalization using Xylem Vue
Brabant Water deployed Xylem Vue to digitalize its network, integrating data for near real-time operational intelligence and non-revenue water management. -
Stadtentwässerung Celle: Wastewater treatment plant process optimization through artificial neural networks
Celle cuts energy consumption by 22% and chemical use by 56% using Xylem Vue WWTP optimization technology, saving tens of thousands of euros annually. -
ApaVital S.A.: Reduction of daily water losses by over 800 m³
ApaVital deploys Xylem Vue to reduce daily water losses by over 800 cubic meters, achieving compliance with EU regulations. -
Hong Kong: development of digital twin pilot for trunk mains water systems in selected areas of New Territories East Region
This project aims to build and calibrate a hydraulic model for trunk mains water systems in selected areas of New Territories East Region and deploy the model through Idrica’s Real-Time What-If-Scenarios solution (now called Xylem Vue).
-
Gruppo CAP: intelligent water network management through advanced analytics and predictive asset planning
Gruppo CAP deployed Xylem Vue's AI-driven platform to optimize its 6,500 km water network, reducing water losses and improving asset management. -
Severn Trent Water: digital twin to optimise energy and emissions in WWTPs
The implementation of a digital twin at the Strongford treatment works has enabled Severn Trent Water to visualise plant performance in near-real time. -
ADI® MBR chosen by speciality potato processor to treat wastewater
Les Aliments Bari Inc.’s processing plant in Saint-Léonard-d’Aston, Quebec, Canada, needed a new wastewater treatment solution. In the past, wastewater was stored in large tanks on-site that was then applied on local farmland when weather permitted.
-
Blog Page
How geothermal and radiant HVAC helped create a net-positive school
In this article, Xylem’s Bell & Gossett highlights its partnership with the Academy for Global Citizenship in Chicago to create a more sustainable school campus.