Documents
-
-
Sanitaire ICEAS SBR technology improves effluent water quality for St. Joseph WWTP
To meet rising environmental standards and prepare for future growth, St. Joseph Sanitary District No. 1 turned to Xylem’s Sanitaire ICEAS® SBR technology. This smart, energy-efficient upgrade replaced aging infrastructure with a modern solution that delivers consistent effluent quality, remote monitoring capabilities, and long-term operational resilience.
-
Scottish Water pledge to make its network as efficient, resilient and cost effective as possible
As part of Scottish Water's asset resilience strategy, it trialled Xylem Concertor, the first wastewater pumping solution with integrated intelligence, at two of its Ayrshire pumping stations: Maple Grove and Cross Dene.
-
Sewerage District relies on PURELAB ® system for BOD testing
Heart of the Valley Sewerage District in Kaukauna, Wisconsin required high-purity water to test plant effluent for biochemical oxygen demand (BOD) and other contaminants. Testing is required to ensure that the effluent meets state and federal guidelines before discharge into the Fox River.
-
Shearer’s Foods treats tough snack food wastewater
Shearer’s Foods is committed to protecting the environment. It has made operational changes to do more with less—less water, less energy, less waste. Its production facilities are state-of-the-art, featuring modern equipment, processes, and systems. The company expected no less when it came to selecting a wastewater treatment solution.
-
-
Silanna Semiconductor turns to Xylem for world-class water solution
Silanna Semiconductor is an Australian company specialised in the design and manufacture of advanced semiconductors. It has established itself as a market leader, providing power control and UVC LED semiconductors to the communications, space, defence, medical, and consumer markets. With dedicated offices in North America, Europe, Asia, and Australia, the company maintains a global presence and ready access to a range of markets and industries.
-
Smartball® Technology Used To Successfully Identify Leaks On Vacuum-Insulated Hot Water Pipeline
Fortum’s core business in Poland is high-efficiency combined heat and power production and heat distribution. The company aims to develop sustainable solutions for cleaner cities, meeting the needs of local communities.
-
Smith-Blair Flanged Coupling Adapter in Central Florida
For this particular job, Smith-Blair built 36 inch Flanged Coupling Adapters (FCAs). The FCAs are designed to provide an efficient means to remove and reinstall the pumps, valves and other fittings during maintenance procedures.
-
-
Utility reduces CSO volume by 80%, saving $400 million in CapEx spending using “smart sewer” technology
Predictive monitoring and automated control optimized combined sewer operations, reducing overflow volumes and deferring major capital infrastructure investment.
-
Southwest Water Reclamation Facility – League City, TX
League City contracted with CDM Smith to manage the expansion project and design and construct a 4.0 MGD (design) / 12 MGD (peak)treatment facility with an energy, labor, and operational efficient process that would meet exceptionally stringent discharge limits. The facility also needed to ensure Type I or Type II non-potable reuse was available for future irrigation and/or amenity use.
-
Splash Lagoon: Improving uptime and efficiency with advanced filtration
Discover how Splash Lagoon, a top 10 U.S. waterpark, improved water clarity and efficiency in its 200,000-gallon wave pool using Xylem’s Defender® filtration system while cutting maintenance, conserving resources, and enhancing guest experience. -
Stadtwerke Trier: optimization of wastewater treatment plant processes thanks to AI
Stadtwerke Trier (SWT) operates the main wastewater treatment plant (WWTP) in Trier, with a capacity of 170,000 population equivalents. This facility was one of the largest energy consumers in the utility for many years, with hundreds of thousands of kilowatt hours of valuable energy being drawn from the public grid as a result of poor control.
-
State of the art water treatment technology for a forging works in Saxony, Germany
Various cooling towers are operated in the water treatment plant at the forge. Disinfection is carried out using expensive biocides, which are also environmentally problematic for rivers when discharged directly. The company was therefore looking for new, efficient and cost-effective disinfection technology to solve these issues. -
-
Stratmoor Hills expands footprint to mitigate PFCs
Since 2018 Stratmoor Hills Water & Sanitation Districts in Stratmoor Hills, Colorado has had two IX48 ion exchange treatment systems in place to remove PFOA and PFOS from two separate wells. Each treatment system was seasonal, running only in the summer and consisted of an ion exchange system from Xylem.
-
Sunlight-blocking covers control algae, reduce operational costs
The Santa Clara Valley Water District (the District) manages an integrated water resources system that includes the supply of clean, safe water, flood protection, and stewardship of streams on behalf of Santa Clara County's 1.8 million residents. The district effectively manages 10 dams and surface water reservoirs, three water treatment plants, an advanced recycled water purification center, a state-of-the-art water quality laboratory, nearly 400 acres (162 hectares) of groundwater recharge ponds, and more than 275 miles (443 km) of streams.
-
Sustainability success for Dairygold: mixers deliver biogas system results that matter
Flygt mixers deliver sustainable success for Dairygold at the heart of the world's largest ADI-BVF® fermenter. Read the case study →
-
-
-
-
Temporary bypass solution maintains treatment operations
Discover how Xylem maintained uninterrupted wastewater treatment during critical screw pump maintenance with a compact bypass pumping system, balanced flow distribution, resilient backup power and 24/7 remote monitoring. -
Temporary Equipment Keeps Power Generating Station Up and Running
CMS Energy needed to design and build a water treatment system to feed the turbines at the 155-megawatt Livingston Generating Station. The system had to withstand extreme cold and satisfy stringent environmental regulations. It also needed to meet a peaking station's intermittent need for reliable demineralized water.