Documents
-
The Orbal® system for biological nutrient removal
Water is precious to the 8000 residents of this town in central Utah, as it is to so many similar places in the arid Intermountain West. Town history attributes Salem City's 19th-century founding to its location as a suitable spot for damming up a local spring to create a pond, which is still the centerpiece of the town.
-
Organic Bottling Facility Ensures Product Integrity with UV Disinfection
Waterborne microorganisms and contaminants of emerging concern such as pharmaceuticals and personal care products in the water are responsible for adverse effects on the flavor, color, odor and shelf life of soft drinks, bottled water and food products. Water used in the food and beverage industry, either for product, or as part of the process must be treated in order to ensure the integrity of the product. Ultraviolet disinfection provides an effective disinfection solution.
-
Ozone Reduces Micropollutants: Bad Sassendorf – The sewage plant of the future
This plant treats water from the Ruhr River to provide drinking water for several million people.
-
Ozone treats polluted groundwater: Xylem’s turnkey containerized solution
This system allows Bayernoil to meet the allowed discharge limit set by the Bavarian authorities into the Danube river.
-
Pennsylvania campground a perfect destination with Goulds Water Technology solution
Since swimming pools and shower facilities are important considerations when campers are selecting a destination, StoneyBrook Estates Campground wanted to ensure that its 30,000-gallon swimming pool and shower house were functioning effectively and efficiently.
-
-
Pet Food Plant Installs Wastewater Treatment System Fit for Humans
New production lines at plant resulted in increase in wastewater flow and load, which exceeded capacity at the municipal plant. Therefore, pet food manufacturing plant needed an on-site wastewater treatment system.
-
Pipeline Inspection of Critical 20-year-old Mine Discharge Water Pipelines in Sensitive Area
In the U.S., mines operate under strict Environmental Protection Agency (EPA) regulations; as such, pipelines must be carefully monitored and maintained.
-
-
-
-
Preventing Rising Main Failures: Leveraging Inspection Data for Proactive Rising Main Management
Most rising mains failures are preventable. And today, inspecting them is easier, more cost-effective, and less disruptive than ever, thanks to the development of advanced inspection technology such as Xylem’s SmartBall.
-
Cleaner water, smarter systems, zero disruption
Pro Club in Bellevue, Washington upgraded its pool system in seven days with advanced filtration and UV technology. The project improved water clarity, air quality, and member experience while saving over 520,000 gallons of water and $134,000 annually.
-
-
-
-
-
Pump replacement project at Gloucester Docks keeps Bristol’s water supply flowing
The four existing column pumps at Gloucester Docks - which are vital for managing water levels in the canal and keeping Bristol’s water supply running - were reaching the end of their working life and needed replacement.
-
Pump Station in Krokom – Unique PE Construction
Xylem delivered a turnkey solution for one of Sweden’s first pump stations featuring a fully integrated PE construction in Krokom. -
Pumps built to stand the test of time
When Paint/Elk Township Sewage Plant installed a Goulds Water Technology submersible effluent pump in the spring of 1991, they would be set for the next two decades.
-
-
Rand Water installs chlorine and ammonia dosing equipment
Klomac, the Southern African agent for Wallace & Tiernan® products, has successfully completed the supply and installation of chlorine and ammonia dosing equipment at Rand Water’s Mapleton Pumping Station as part of that station’s upgrading and expansion programme. The Wallace and Tiernan equipment includes four Model V2000™ automatic chlorinators rated at 40 kg/h each, four ammonium hydroxide dosing pumps and GMS chlorine gas leak detection equipment.
-
Realtime monitoring cuts pollution risk at Scottish Water site
When a critical pumping station failed, Scottish Water used Xylem Vue Secure Connect monitoring and real-time data to restore resilience and protect the environment. -