Parece que vem de United States, mas o site atual que selecionou visitar é Portugal. Pretende alterar os sites?

Sim. Não. Mantenha-me no site atual.

Documents

Documents

  • Integrated Device Manufacturing

    Integrated device manufacturing requires water and wastewater solutions designed specifically for the types, geometries and chemistries of the devices being...
  • Silicon & Polysilicon

    Purity of the silicon wafer substrate has an impact on the ability of integrated device manufacturers to maintain and/or increase yields. With geometries...
  • Oil & Gas

    Rising operational costs, low oil prices, and the need to maintain production levels to ensure cost efficiency are ongoing challenges faced by the oil and gas...
  • Industrial Gas Production

    Industrial gases such as hydrogen, nitrogen, and oxygen are key feedstocks for the petrochemical and agrochemical industries. They are used in the production...
  • Ash Pond Dewatering

    Solutions to meet coal combustion residuals (CCR) compliance with ash pond closures.
  • Ballast Water Treatment

    For over a century, ships have used water as ballast to provide stability, making ballast water essential to safe and efficient shipping. However, ballast...
  • Boat Engine Cooling

    Unlike a car motor, boat engines use the cool water from below the vessel to keep cool. There are two main types of marine cooling systems that boat engine...
  • Clinical Chemistry and Diagnostics

    Water purity is crucial in the fields of clinical chemistry and diagnostics. Ongoing developments in the approach to clinical testing and in the sophistication...
  • Dairy Wastewater Treatment

    In milk and cheese production, the required quality of process water and the accompanying clean-in-place (CIP) process produces a harsh effluent with varying...
  • Dry Dock Drainage

    A dry dock is a basin used for the construction, repair and maintenance of ships, boats and other vessels. The dock can be flooded to allow the vessel to float...
  • Greywater Draining

    Greywater is the untreated water from your onboard sinks, showers, washing machine, dishwasher, and the wastewater from cleaning your boat with detergents,...
  • Hydro Jetting for Marine Construction

    Support marine construction hydro jetting projects with high-head pump systems for structural cleaning and concrete preparation in freshwater and saltwater...
  • Industrial Dewatering

    In industrial applications, water used in processing, cleaning, and emission controls may result in both water and solids that may be contaminated....
  • Industrial Water Recycle & Reuse

    Industrial water reuse and recycling is the process by which wastewater produced from one source is treated to be reused in the same process or recycled for...
  • Iron and Manganese Removal

    Iron and Manganese Levels in Your Water The recommended levels of 0.3 mg/L Fe and 0.05 mg/L Mn correspond to concentrations above which iron and manganese will...
  • Laboratory Water Purification

    When it comes to laboratory grade water, Xylem is your trusted partner for high quality water purification systems. We can provide a range of solutions to meet...
  • Lighting Control

    From locating buoys to illuminating a narrow channel or even searching for a person overboard, marine searchlights must perform a range of tasks. This is why...

Create Wishlist

Add to wishlists
Select one or more wishlists.

Item successfully added to wishlist.

Item successfully added to new wishlist.
Item successfully added to existing wishlist.