It looks like you are coming from United States, but the current site you have selected to visit is Sweden. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Enable high contrast mode

Sökresultat

Sökresultat

  • High Performance Materials

    Production of high performance materials used in the fabrication of semiconductors has been evolving to meet increasing quality needs of the device...
  • Integrated Device Manufacturing

    Integrated device manufacturing requires water and wastewater solutions designed specifically for the types, geometries and chemistries of the devices being...
  • Silicon & Polysilicon

    Purity of the silicon wafer substrate has an impact on the ability of integrated device manufacturers to maintain and/or increase yields. With geometries...
  • Municipal Drinking Water

    Water utilities and municipalities face numerous challenges in their efforts to provide clean and safe drinking water to communities. From aging infrastructure...
  • Oil & Gas

    Rising operational costs, low oil prices, and the need to maintain production levels to ensure cost efficiency are ongoing challenges faced by the oil and gas...
  • Hydraulic Fracturing

    Water is essential to your operation, but managing it presents numerous challenges. You need to source millions of gallons, utilize it in the extraction...
  • Offshore Oil & Gas Water Management

    Oil and gas customers rely on Xylem’s application expertise, which comes from decades of experience, to solve water challenges in offshore environments. From...
  • Industrial Gas Production

    Industrial gases such as hydrogen, nitrogen, and oxygen are key feedstocks for the petrochemical and agrochemical industries. They are used in the production...
  • Ash Pond Dewatering

    Solutions to meet coal combustion residuals (CCR) compliance with ash pond closures.
  • Ballast Pumping

    When you're having fun on a wakeboard, skis, or a tube, a bigger wake will create a more exhilarating ride, and today's modern ballast pumping systems make...
  • Ballast Water Treatment

    For over a century, ships have used water as ballast to provide stability, making ballast water essential to safe and efficient shipping. However, ballast...
  • Barge Ballasting & Jetting

    Barge ballasting and jetting systems ensure stable barge positioning during loading, unloading, and transport, and support marine construction with jetting for...
  • Biological Wastewater Treatment

    Biological wastewater treatment is an economical means of removing both organic and inorganic contaminants from wastewater. While it is commonly used for the...
  • Boat Engine Cooling

    Unlike a car motor, boat engines use the cool water from below the vessel to keep cool. There are two main types of marine cooling systems that boat engine...
  • Clinical Chemistry and Diagnostics

    Water purity is crucial in the fields of clinical chemistry and diagnostics. Ongoing developments in the approach to clinical testing and in the sophistication...
  • Cooling Tower Water Treatment

    Industries utilize cooling towers to maintain heat transfer surfaces and enable process heat removal and product throughput. In commercial or building...

Create Wishlist

Add to wishlists
Select one or more wishlists.

Item successfully added to wishlist.

Item successfully added to new wishlist.
Item successfully added to existing wishlist.