It looks like you are coming from United States, but the current site you have selected to visit is China. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Water usage optimization in biofiltration odor systems

Improving water resiliency with an alkaline supplement

White Paper: Water usage optimization in biofiltration odor systems

Water scarcity is a growing concern in today’s environment with increasing water needs and limited access to resources. This white paper explores the use of an alkaline supplement to improve water resiliency in a Biotrickling filtration system for more sustainable operation.

The goal of this project was to maintain optimal pH in a Biotrickling filtration system (BTF) while reducing water usage. Normally, pH is maintained using a continual stream of fresh water into the BTF. Evoqua demonstrated that an alkaline addition can significantly reduce the amount of water needed without impacting system performance. 

This was accomplished using a 3-stage 3.7 m (12 ft) diameter BTF operating at 283 m3/min (10,000 ft3/min), using 50% caustic soda (sodium hydroxide) as the alkaline material in conjunction with a pH control system. Initial water usage at the site was 64 L/min (17 gpm) on average. After addition of caustic soda and utilizing pH control, the water usage dropped to an average of 19 L/min (5 gpm), a 70% reduction, while maintaining previous levels of hydrogen sulfide removal.