-
Xylem installs a flexible, high-efficiency surface water pumping system
Delta Sand & Gravel Co., located in Eugene, Oregon, has been providing quality aggregate materials, service and expertise for almost nine decades. The company offers a full line of aggregate products for year-round, all-weather construction and demolition landfill. Xylem has partnered with Delta Sand & Gravel since 2013, to provide holistic water management solutions.
-
Xylem Delivers Actionable Data Within a Tight Time Frame to Enhance the Safety and Resilience of a Nuclear Power Plant
A condition assessment helps to understand the state of the prestressing wire which provides the pipe’s strength. PCCP manufactured during the 1970s is prone to low ductility in the wire and susceptibility to hydrogen embrittlement, both of which increase the risk of failure. Worn PCCP can rupture with no warning, potentially shutting down the entire facility.
-
Pipeline Inspection of Critical 20-year-old Mine Discharge Water Pipelines in Sensitive Area
In the U.S., mines operate under strict Environmental Protection Agency (EPA) regulations; as such, pipelines must be carefully monitored and maintained.
-
Integrated Water Management System Supports 15% Increase in Production at Aggregates Processing Plant
One of the largest U.S. producers of construction aggregates decided to relocate their processing plant to facilitate increased production capacity. However, the new location was further away from the plant’s water supply.
-
Xylem’s holistic solution of mixers and pumps supports efficient mine slime transport – from sump to surface disposal
One customer, operating a hard rock nickel mine in Ontario, needed an efficient and reliable solution to transport its mine slime from an underground sump back to the surface while ensuring continuity in production and minimizing downtime.
-
Remote Pumping Solution helps Mine Operators Reach New Depths in Harsh Environment
A customer in Perú needed to drain water as its large open-pit mine operation reached as deep as 1,200 ft (365 m) below the surface. The discovery of more copper in the mine, and an expected excess of water during rainy summer months also prompted the company to act. They sought a remote solution for monitoring and controlling their pumping system, particularly as routing electrical power became more difficult the deeper they dug....
-
Xylem partners with Hometown H2O to install water well for retired Oregon couple
For 34 years, Steve and Lana Gleason made due without a traditional residential water system. The couple, who live in the rural logging community of Jewell, Oregon, pumped water for washing from a nearby river and made 40-mile round trips from their home to haul drinking water from a spring.
-
Three thousand assets from the Municipality of Ede in XDM
The Municipality of Ede comprises ten residential nuclei located in one of the most beautiful, wooded parts of the Netherlands. A total of more than two thousand pumping stations have to be managed and maintained there, for which a maintenance management program is used.
-
Xylem’s Flygt Concertor Saves $20,000 Per Year in Maintenance Costs at Coal Fired Power Plant
Operators of one of the largest coal fired power plants in the US based in Michigan, were looking for an efficient, robust and reliable pumping solution to move sludge water from each of the plant’s four sumps.
-
Cleaning of disc diffusers makes Prochamp’s wastewater treatment greener
Soon after starting this biological treatment method, the membrane disc diffusers were found to be clogged with scale particles. However, this problem was satisfactorily solved by the Xylem’s mobile cleaning service: the Diffuser Liquid Cleaning Service.
-
Real-time decision support helps cut combined sewer overflow volume by 100 million gallons and reduces capital needed for regulatory compliance
Evansville is located on the north bank of the Ohio River in southwest Indiana. The City’s sewer system, parts of which are more than 100 years old, serves a population of 163,000, with combined sewers making up almost 40 percent of the total sewer area.
-
Engineering a more efficient way to source and transfer water
One of the largest global energy exploration companies faced the challenge of drawing source water among the steep slopes of Northern Pennsylvania. The water had to be drawn from a 30-feet deep wet well beside a creek and then pumped 300-feet vertically out of a ravine into the impoundment pond.
-
Xylem’s Advanced Remote Monitoring Saves $25,000 per Month in Labor Costs and Reveals Cost Savings
According to Deloitte LLP., large U.S. producers with significant shale oil and gas operations reported operating margins averaging around 20 percent in 2012, a significant drop from 2006 operating margins of 45 percent.
-
The Smarter Water Manager
Communities around the world are facing a growing storm. Complex challenges including water scarcity, changing demographics, extreme weather patterns, and aging or overly stressed infrastructure are colliding to threaten critical water, energy, transport, enterprise and health networks. The water industry is in the eye of the storm.
-
Supervision of pumping stations in Vlaardingen is highly effective
In the municipality of Vlaardingen, rainwater and wastewater are processed by more than seventy pumping stations, six of which are large, dry-installed main pumping stations and a large number of subsidiary and mini-pumping stations. Supervision is the responsibility of Xylem, which means that the Vlaardingen maintenance department receives a weekly overview of all relevant events.
-
Xylem’s quick response restores critical water supply to North Carolina community during COVID-19 outbreak
Xylem Rental Solutions helped a North Carolina community restore water service quickly during the COVID-19 outbreak with a temporary replacement, using a Flygt submersible pump, after a permanent pump failed.
-
-
XDM software tested in municipality of Goes, the Netherlands
Xylem carries out the maintenance of wastewater pumping stations on a contract basis for a large number of municipalities in the Netherlands. With the maintenance contracts in place, Xylem is in regular contact with the associated technical people to share new solutions and insights.
-
Focusing on Resilience in the Face of Emerging Contaminants
There are over 150,000 public drinking water systems in the United States and more than 80 percent of the population receives their potable drinking water from these systems.
-
Remote Bathymetric Survey in Kalgoorlie Mine Pits, Australia Using an Unmanned Radio-controlled Boat
Surveys were conducted at three mining pits in January 2018 using the Xylem UK rQPOD radio controlled vessel and the SonTek HydroSurveyor-M9 system over two days. Speed of sound in water cor- rections, an integral part of any acoustic survey, were carried out using the SonTek CastAway-CTD. HYPACK software managed the prepara- tion, survey, processing and outputs for the survey.
-
Xylem’s Standard Xchange Brand helping Make Cheap, Green Fuel a Reality
This pioneering pump turns feedstock like cheap sugar into clean-burning ethanol fuel that emits far less greenhouse gases into the atmosphere than oil-based gasoline. It’s designed to be installed in household driveways and the parking lots of small businesses.
-
-
-
Smartball® Technology Used To Successfully Identify Leaks On Vacuum-Insulated Hot Water Pipeline
Fortum’s core business in Poland is high-efficiency combined heat and power production and heat distribution. The company aims to develop sustainable solutions for cleaner cities, meeting the needs of local communities.