It looks like you are coming from United States, but the current site you have selected to visit is Japan. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Enable high contrast mode

Flygt pumps reduce energy cost by 31 percent thanks to N-Technology

USA

Challenge
In the spring of 2012, a sewage lift station in the City of Bathurst was requiring monthly servicing to pull the pumps and remove thick fibrous clogs. Although the city’s utility had a service truck with a lift, each service call required the rental of a boom truck due to the weight of the pumps undergoing maintenance.

Solution
The Flygt N-Pump with TotalCare Services Xylem proposed the Flygt N-technology N-3171 pump (435MT 25HP) to replace the existing competitor’s 20 HP submersible sewage pumps that were in service for a little over a year. Advantages of Flygt N-technology pumps include clogfree pumping, an innovative self-cleaning impeller and a flexible and modular design, which ensures sustained efficiency. Flygt N-pumps are also backed by Xylem TotalCare services for secure operations.

Download Case study