It looks like you are coming from United States, but the current site you have selected to visit is Singapore. Do you want to change site?
Xylem’s highly efficient pumps will create additional capacity to help manage Combined Sewage Overflows and capture, transport and treat increased amounts of wastewater
Washington, DC (February 9, 2023) – The Toronto, Ontario metropolitan area has seen rapid population growth over the last several decades and has also developed a Wet Weather Flow Master Plan that aims to virtually eliminate Combined Sewage Overflows (CSO) from the sewage collection system.
To support this expansion, Xylem (NYSE:XYL), a leading global water technology company, has been selected by the City of Toronto to supply customized equipment for a new integrated pumping station (IPS) – a critical component that ensures reliable and safe transport of wastewater. The project will replace two existing pumping stations, one operating since 1911 and the other since the early 1970s, both adjacent to the Ashbridges Bay Wastewater Treatment Plant.
The plant’s new IPS will include 14 Flygt A-C series dry pit pumps. These pumps, designed for low maintenance and operational costs, will reduce Toronto’s energy consumption rate and ensure reliable station operation.
“As Toronto continues to grow, we are proud to support such a large and complex project,” said Matthew Pine, Chief Operating Officer, Xylem. “Xylem’s highly efficient solutions, expertise and local presence will help ensure safe, reliable and sustainable wastewater treatment for generations to come.”
Once operational, this IPS will move raw sewage from the underground sewer system into the treatment plant. In addition, the IPS will add Wet Weather Flow pumping capability to pump collected CSOs from the new Don River and Central Waterfront tunnel system, to a new high-rate treatment facility.
Xylem’s Pewaukee, Wisconsin facility will design, build and test the customized equipment. Life cycle services will be provided by Xylem’s three Service Centers near Toronto in Etobicoke, Ottawa and Sudbury. Certified and factory-trained technicians will provide the necessary expertise for installation, training, monitoring/diagnostic and maintenance.
The project is currently in its design stage; construction is expected to start in 2025 and take ten years to complete.
Xylem (XYL) is a leading global water technology company committed to solving critical water and infrastructure challenges with innovation. Our more than 17,000 diverse employees delivered revenue of $5.5 billion in 2022. We are creating a more sustainable world by enabling our customers to optimize water and resource management and helping communities in more than 150 countries become water-secure. Join us at www.xylem.com.
Kim Genardo
+1.919.417.2760
kim.genardo@xylem.com