Analytics

Make well-founded decisions based on historical data

Secure Connect shows live data and connectivity status for the connected devices. The application stores the data and trend graphs are shown for analysis of the data over time.

In the station analytics, time series are shown for different data points. Through the chart settings, it is possible to visualize the station events below the time series. The feature allows users to correlate the data and a specific event.

To get an overview of the different events that have ocurred over a time period, the analytics page provides event count charts. Events can also be visualized in a data point time series.

The user can choose resolution, down to the lowest resolution of 1 min. This is limited by the connectivity of the station, not the device installed. If the resolution is set to 1 min, data should update at least every minute. If the resolution is set to 10 min, 1 hour or longer the data update is also expected to take longer.

Visualize and compare data points in charts

Analytics has different graph-types available. These are data point plots, counter deltas, and state count and utilization. The types of graphs available depend on the configuration of the station and the devices and sensors  installed. The graphs can be combined in the same chart for comparison. On the analytics page it is also possible to view historical data and download all the live data into a single CSV file.

Export the data for analysis in other tools

The user selects which charts to show and it is possible to export the data for further analysis outside the application.

Related FAQs

Many users have had similar questions about Analytics, Live Data, API and OPC UA Connector.