It looks like you are coming from United States, but the current site you have selected to visit is Oman. Do you want to change site?

Yes, please! No, keep me on the current site

Custom Devices

Devices that are not on the list of compatible devices can be added as custom devices. The user defines the device type and the data points. Secure Connect uses the information about the data points for analytics and to visualize the data from the device.

Requirements

  • All devices that connect to the gateway with one of the following options must use the same communication interface:
    • RS-232
    • RS-485
    • Ethernet
  • All connected devices must be of the same type.
    • This requirement does not apply to I/O devices.
    • It is possible to have different SENECA devices connected to the same gateway. It is not possible to have a SENECA device and a device of a different type connected to the same gateway.
Connection Maximum number of connected devices for each
gateway
RS-232 8
RS-485 8
Ethernet 4

Questions?

Many users have had similar question about the CCD 401 gateway.
Look for answers in the
Connectivity Frequently Asked Questions