It looks like you are coming from United States, but the current site you have selected to visit is Oman. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Enable high contrast mode

How to clean the remote tank switch

Like the S1-200 pump, the Remote Tank Switch should not be used in extremely dirty, sandy or muddy water. If the pump is operated with liquid under normal conditions, it should not be necessary to clean the Remote Tank Switch.

For more information read the following article:

Tolerable salt and sand content

Required tools

  • Screwdriver (crosshead)

Disassembly

  1. Remove the four screws on the top of the Remote Tank Switch with a crosshead screwdriver.
  2. Remove the gasket and make sure it is not broken and if necessary wash it.
  3. Remove the paddle and make sure the spring is not jammed. If necessary rinse or clean it.
  4. Check that the inside of the Remote Tank Switch is free of any obstruction. If necessary wash or clean it.
  5. In case it is damaged, it must be replaced. Contact your authorized distributor.

Assembly

  1. Make sure that the paddle spring moves in the same direction as the flow inlet, note that a wrong assembly will not allow the Remote Tank Switch to work properly.
  2. Put the gasket back in place.
  3. Make sure that the direction of the arrow on the Remote Tank Switch matches the direction of the arrow on the non-return valve (as well as the fluid) and tighten the top chamber with the four screws. Apply a torque of xxxx n.m.
     

You can see the previous steps in the following video: