It looks like you are coming from United States, but the current site you have selected to visit is Qatar. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Xylem Vue Secure Connect Remote Access FAQs

Remote inspection

  1. Go to Stations.
  2. Select a station.
  3. Go to Inspections.
  4. Click the Start new inspection round button.
    Secure Connect starts a new inspection round.
  5. To exit the inspection round, click the Exit inspection round button.

  1. Go to Stations.
  2. Select the station.
  3. Go to Inspections.

Secure Connect lists the inspection history.

With the Remote inspection service, the user can start an inspection round. The inspection round guides the user through each station that is related to the customer. After a detailed station checkup, or a brief look at the station overview, the user marks the station as inspected. The user can also write a description. The inspections are logged, and the inspection history is available for each station.

Only Xylem personnel can enable this service.

  1. Go to Admin > Customers.
  2. Select the customer.
  3. Click Edit.
  4. In the Services section, check the Remote inspection option.
  5. Click the Save button.

Secure Connect makes the Remote inspection service available for the stations that are related to the customer. By default, Xylem personnel are allowed to do remote inspections.

  1. Go to Admin > Customers.
  2. Select the customer.
  3. Go to the Xylem control tab.
  4. Click the Remote inspection switch.
  5. Click Save.

Secure Connect prevents Xylem from doing remote inspections.

Remote control

  1. Go to Stations.
  2. Select a station.
  3. Go to Settings.
  4. Go to the Services tab.
  5. Click the Remote control switch.

Secure Connect enables remote control of the applicable devices in the station.

  1. Go to Admin > Customers.
  2. Select a customer.
  3. Click Edit.
  4. In the Services section, check the Remote control option.
  5. Click the Save button.

Secure Connect makes the Remote control service available for the stations that are related to the customer.

This setting is available when the Remote control service is enabled for the related customer.

  1. Go to Admin > Customers.
  2. Select a customer.
  3. Go to the Xylem control tab.
  4. Click the Remote control switch.
  5. Click the Save button.

No, only you and Xylem can control your assets if the remote control service is enabled. Xylem never uses the remote control without your approval.

For instructions on how to allow Xylem to control devices remotely see:
How do I allow Xylem to control devices remotely?

  • APP 411
  • Digital Output
  • EcoTouch
  • FGC 313/323
  • FGC 401/411/421
  • Hydrovar HVL
  • Hydrovar X
  • LC150
  • Multismart
  • Nexicon (Remote mode in HMI)
  • PS 220

Remote control operations are only supported by the CCD 401.

APP 411

  • Reset alarms
  • Set start level
  • Set stop level
  • Set high level
  • Set speed
  • Set power
  • Set auto mode
  • Set off mode
  • Start pump cleaning


Digital output

  • Set high
  • Set low


Ecotouch

  • Disable remote signal
  • Enable remote signal
  • Set full power function off
  • Set full power function on
  • Set design flow
  • Set design UV transmittance


FGC 313/323

  • Remote block
  • Revert to auto
  • Set high level
  • Set start level
  • Set stop level
  • Reset alarms


FGC 401/411/421

  • Set off mode
  • Set auto mode
  • Set semi-auto mode
  • Reset alarms
  • Set start level
  • Set lag start level
  • Set stop level
  • Set high level


Hydrovar HVL

  • Set required value
  • Set start value

Hydrovar X

  • Pump on
  • Pump off
  • Set start value
  • Auto start enable
  • Auto start disable
  • Error reset

LC150

  • Stage 1 - Set low
  • Stage 1 - Set high
  • Stage 2 - Set low
  • Stage 2 - Set high
  • Stage 3 - Set low
  • Stage 3 - Set high
  • Stage 3 - Set high
  • Pump 1 - Set AUTO
  • Pump 2 - Set AUTO
  • Pump 3 - Set AUTO
  • Pump 1 - Set HAND
  • Pump 2 - Set HAND
  • Pump 3 - Set HAND
  • Pump 1 - Set OFF
  • Pump 2 - Set OFF
  • Pump 3 - Set OFF


Nexicon

  • Inhibit pump enabled.
  • Inhibit pump disabled.
  • Set Speed.
  • Set power.
  • Start pump cleaning.
  • Reset alarms.
  • Set start level.
  • Set stop level.
  • Set high level.
  • Start pumping cycle.
  • Stop pumping cycle.
  • Inhibit station enabled.
  • Inhibit station disabled.

 

Multismart

  • Set pump to Auto
  • Set pump to Manual
  • Set pump to Off
  • Set Start level
  • Set Stop level
  • Set Activation/Deactivation point for Level High
  • Set Activation/Deactivation point for Level High High
  • Set Activation/Deactivation point for Level Low
  • Set Activation/Deactivation point for Level Low Low


PS 220

  • Set auto mode
  • Set off mode
  • Reset pump
  • Set start level
  • Set stop level
  • Set reference

  • The regional area where the CCD is installed must have law and regulations that allows remote control of pumps, digital outputs, or other remote control functions.
  • The customer has the subscription to the remote control service under Admin>Customer.
  • The controller or device is included on the list “Which devices can Secure Connect control remotely?“

Remote control device-specific operations

  • Reset alarms
  • Set start level
  • Set stop level
  • Set high level
  • Set speed
  • Set power
  • Set auto mode
  • Set off mode
  • Start pump cleaning
  • Digital output
  • Set high
  • Set low

  • Disable remote signal
  • Enable remote signal
  • Set full power function off
  • Set full power function on
  • Set design flow
  • Set design UV transmittance

  • Remote block
  • Revert to auto
  • Set high level
  • Set start level
  • Set stop level
  • Reset alarms

  • Set off mode
  • Set auto mode
  • Set semi-auto mode
  • Reset alarms
  • Set start level
  • Set lag start level
  • Set stop level
  • Set high level

  • Set required value
  • Set start value

  • Inhibit pump enabled
  • Inhibit pump disabled
  • Set Speed
  • Set power
  • Start pump cleaning
  • Reset alarms
  • Set start level
  • Set stop level
  • Set high level
  • Start pumping cycle
  • Stop pumping cycle
  • Inhibit station enabled
  • Inhibit station disabled

  • Set auto mode
  • Set off mode
  • Reset pump
  • Set start level
  • Set stop level
  • Set reference