It looks like you are coming from United States, but the current site you have selected to visit is Yemen. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Enable high contrast mode

Secure in-field firmware updates to support more resilient connected products

EU Cyber Resilience Act case study

Context 

For manufacturers of connected products, cybersecurity is no longer just a technical consideration. The EU Cyber Resilience Act (CRA) makes it a legal one. From September 2026, manufacturers must meet active vulnerability reporting obligations, with full enforcement following in December 2027.

Sentec supported an industrial customer in implementing secure in-field firmware update capability for a product based on a new embedded processor platform. The goal was to enable firmware updates in the field while protecting intellectual property, preserving device integrity, and ensuring that only trusted firmware could be installed. 

Challenge

For products that need to be updated after deployment, firmware update capability must be balanced with strong security controls. The customer needed a solution that would ensure: 

  • Only firmware cryptographically signed by the customer would be accepted by the device
  • Firmware files remained encrypted in transit and at rest
  • Unauthorised users could not access the system's internal data

These requirements map directly onto CRA obligations around secure update mechanisms, vulnerability management, and access control. This is increasingly a baseline expectation from both regulators and buyers. 

The project was made more demanding by the fact that the product used a relatively new processor platform. While the platform included hardware-level support for encryption, along with vendor-supplied software and firmware libraries for encryption and authentication, it did not support in-field upgrades out of the box.

“Writing complex firmware requires perseverance, expertise and attention to detail. Sentec is able to offer all of these.”
Dr. Steve Melnikoff, Staff Software Engineer, Sentec

Solution 

Sentec developed a secure approach to in-field firmware updates by combining the processor's built-in security capabilities with a carefully designed update mechanism tailored to the customer's product. 

The delivered solution enabled:

  • Encrypted and authenticated firmware images to be transmitted to the device
  • Firmware to be verified, decrypted, and stored securely on receipt
  • Automatic rejection of invalid updates where data was corrupted or authentication was missing
  • Protection against unauthorised access to the processor's internal data 
  • Rollback to the previous valid firmware version if a new version failed during first startup

Delivering this required more than integration work. Sentec identified and fixed bugs in the vendor-supplied firmware and reported them to the manufacturer for inclusion in future releases. The undocumented hardware behaviour required direct collaboration with the vendor's engineering team. Both steps went beyond the original project scope but were necessary to produce a solution that would hold up in a deployed product environment.

Outcome 

For the customer, this delivered a defensible, auditable mechanism for managing firmware vulnerabilities in deployed devices. That is precisely what the CRA requires manufacturers to demonstrate.

The resulting firmware met the customer's functional and security requirements in full. Testing verified that the secure update process worked as intended. Any deviation from the expected update conditions (corrupted data, missing authentication, or an unrecognised firmware signature) would prevent the update from taking place. Testing also confirmed that unauthorised access to internal processor data was not possible without proper authorisation, and that the system could safely revert to the previous firmware version if a new update failed to run. 

Conclusion 

This engagement demonstrates what genuinely secure firmware development looks like when the platform is new, the documentation is incomplete, and the stakes are real. Resolving undocumented hardware behaviour and vendor firmware bugs required embedded expertise, direct manufacturer engagement, and a willingness to go beyond the original brief to get the outcome right.

For manufacturers building connected products today, secure in-field update capability is a CRA requirement rather than an optional enhancement. Products that cannot be updated safely in the field will become progressively harder to maintain, certify, and defend.

Sentec guides manufacturers through that transition, working from their existing platform outward. Rather than imposing a prescribed architecture, the team assesses what the client's hardware and firmware base can support, identifies the gaps that matter most for CRA compliance, and builds a route forward that is both technically sound and sustainable. Getting that foundation in is significantly less costly than retrofitting it under regulatory pressure.

Back to Top