-
Article
Ridurre le perdite idriche senza rifare la rete: il ruolo di hydrovar® X+ e HVX+ Smart Card Controller nelle grandi reti acquedottistiche
Scopri come hydrovar® X+ e HVX+ Smart Card Controller aiutano i gestori idrici a ridurre le perdite di rete (NRW), ottimizzare la pressione e migliorare l’efficienza energetica senza rifare gli acquedotti. -
Article
The driving force behind steel: Innovative pump technology
Discover how Lowara pump technology supports cooling, water reuse, pressure boosting, and energy-efficient water management in steel and metals plants. -
Article
Mixing limited conditions: A big problem with a simple solution
In aerobic process tanks, aeration equipment is conventionally designed to both deliver oxygen for biological treatment (process oxygen demand) and mix the contents of the basin. -
Article
EnviroMix BioMix-DC system earns WEF innovative technology award
EnviroMix’s BioMix-DC Enhanced Anaerobic Mixing System was selected as a 2022 WEF Innovative Technology Award winner. -
Article
The revised Urban Wastewater Treatment Directive: Why it’s time to act
Learn how wastewater treatment plants can prepare for the revised UWWTD, improve performance and unlock long-term operational benefits with Xylem. -
-
Article
HVAC energy efficiency: reducing consumption in existing systems with advanced control technologies
Strategies and technologies for modernising heating and cooling systems in residential and commercial buildings. -
Article
How total water management supports dairy processing growth
Learn how total water management helps dairy processors expand production, optimize wastewater treatment, reduce costs, and prepare for changing regulations. -
Article
Rising electricity demand makes water reliability critical for nuclear power
Learn how water treatment, ion exchange resin, and expert technical support help nuclear power plants improve reliability, maximize uptime, and meet growing electricity demand. -
Article
5 errori nella scelta di una pompa da pozzo
Le criticità più comuni negli impianti edilizi e come evitarle fin dalla progettazione -
-
Article
Three ways hydronic systems benefit data centers
From lower energy consumption to maximum uptime, modern hydronics deliver substantial advantages -
Article
Oltre la pompa: come i circolatori intelligenti stanno trasformando le prestazioni degli impianti HVAC
Con la diffusione di pompe di calore, sistemi ibridi e applicazioni a portata variabile, le installazioni non sono più prevedibili come un tempo. -
Article
The cost you’re not measuring. How best-in-class efficiency minimises total cost of ownership
When pumping systems are not optimised (oversized duty points, fixed-speed operation, poor hydraulic matching to the actual load profile) every hour of operation is an hour of unnecessary electricity spend. -
Article
Il costo che non state misurando. Come l'efficienza top di gamma riduce al minimo il TCO
Campagna di upgrade delle pompe Lowara -
Article
PFAS e tecnologia delle pompe: fare chiarezza sulla complessità per i gestori del servizio idrico
-
Article
Basta rincorrere i guasti: la manutenzione programmata che fa la differenza
Un approccio strutturato alla manutenzione consente di ridurre i costi nascosti, prevenire i fermi impianto e migliorare la continuità operativa nel lungo periodo. -
Article
La normativa sulle acque sotterranee si fa più stringente: cosa cambia con la nuova direttiva UE per gli operatori di pozzi – e perché il controllo della pompa è decisivo
Con l'adozione della Direttiva (UE) 2026/805, l'Unione Europea ha rafforzato in modo significativo il proprio quadro normativo per la protezione della qualità delle acque, sottoponendo le falde idriche a un livello di controllo senza precedenti. -
Article
Three ways liquid cooling presents an opportunity for water use efficiency
ebook explores how liquid cooling can help data centers meet growing AI-driven demands while improving water and energy efficiency through a a system-level approach. -
Article
Powering the HVAC transition: how xylem is enabling the next generation of low-carbon buildings
As energy performance requirements tighten, the need for ultra-efficient pumping solutions is growing fast. Xylem’s ecocirc S, M and L circulators meet this challenge head-on. -
Article
Future-proofing data centres starts when minimum compliance stops
Data centres are under growing technical, regulatory and public pressure. Energy, water and carbon aren’t side issues to manage after commissioning. -
Article
Customer-driven innovation in pharmaceutical water generation
Discover how Xylem's MemGEN™ water generation solution addresses the core challenges of pharmaceutical water systems—lead times, cost control, compliance, and serviceability—through customer-driven design. -
Article
Reflui civili: come scegliere tra pompe sommergibili e trituratori
Nella gestione dei reflui civili, la scelta della tecnologia di pompaggio non è mai neutra. -
Article
Resilienza idraulica urbana: perché il drenaggio è diventato un’infrastruttura critica
Scopri perché il drenaggio urbano è diventato un’infrastruttura critica e quali soluzioni tecniche adottare di fronte a eventi climatici estremi.