-
Emergency sewer system repair
40-year-old carbon steel pipe with catastrophic failure repaired in hazardous wet well conditions. Smith-Blair 675 restored system integrity with zero downtime. -
Pump Station in Krokom – Unique PE Construction
Xylem delivered a turnkey solution for one of Sweden’s first pump stations featuring a fully integrated PE construction in Krokom. -
Eau d’Azur: France’s first smart water network cuts losses and strengthens drought resilience
The Metropolis of Nice is implementing a hypervision platform, based on Xylem Vue technology, to increase efficiency, sustainability, and resilience by providing a real-time view of the network. -
Thames Water and Xylem set new standard for pump upgrades at scale
A Xylem and Thames Water partnership represents a shift in how water companies can manage inherited infrastructure. -
Scottish Water cuts energy by 60% with Flygt Concertor intelligent pump system
Scottish Water partnered with Xylem to upgrade hundreds of pumping stations with innovative, energy-efficient technology, as part of its commitment to reaching net-zero emissions. -
Un piccolo comune è riuscito a risparmiare 3.000 euro e 7.500 kg di CO₂ all’anno sostituendo una vecchia pompa.
Lichtenau è un piccolo comune di 3.600 abitanti. Il sistema idrico locale fornisce ogni anno 170.000 m³ di acqua a 1.300 abitazioni. L’azienda Augustin, con sede a Gunzenhausen e partner di vendita e assistenza Lowara, supporta da tempo il comune offrendo consulenza e proponendo soluzioni di pompaggio più economiche e innovative grazie al know-how Lowara.
-
-
Xylem bypass system helps facilitate pump station upgrades
Allegheny County Sanitary Authority (ALCOSAN) is a municipal authority that provides wastewater treatment services to 83 communities, including the city of Pittsburgh, reaching a total population of 1.2 million people. -
Welsh Water scales up Xylem’s Flygt Concertor for smarter wastewater management
Dŵr Cymru Welsh Water is scaling up its deployment of Flygt Concertor intelligent pumping systems to improve wastewater network resilience, reduce energy consumption, and support its environmental goals. -
State of the art water treatment technology for a forging works in Saxony, Germany
Various cooling towers are operated in the water treatment plant at the forge. Disinfection is carried out using expensive biocides, which are also environmentally problematic for rivers when discharged directly. The company was therefore looking for new, efficient and cost-effective disinfection technology to solve these issues. -
Nanobubbles enable Meister Cheese to increase cheese & biogas production
Meister Cheese improved wastewater treatment and biogas production using Moleaer's nanobubble technology, saving $10M in CAPAX improvements and doubling cheese output. -
Foul odors eliminated using nanobubble technology at a poultry processor
Miller Poultry cut foul lagoon odors and improved water quality using Moleaer's nanobubble technology, solving odor issues and boosting treatment efficiency. -
Maximizing biogas production through effective mixing technology and active seal protection
Learn more about maximizing biogas production through effective mixing technology and active seal protection. Read our case study with our customer Nesemeier now →
-
Sustainability success for Dairygold: mixers deliver biogas system results that matter
Flygt mixers deliver sustainable success for Dairygold at the heart of the world's largest ADI-BVF® fermenter. Read the case study →
-
Xylem‘s Bell & Gossett and the Academy for Global Citizenship make a powerful investment in education and community
How could more energy, ideas and creativity be created than what is consumed? That is the broader vision behind AGC’s focus on being the most sustainable school of the Midwest, where everything from the classroom to the cafeteria contributes to a climate-friendly output. -
Le pompe Xylem Lowara garantiscono prestazioni d’eccellenza nel grattacielo più alto del mondo
Ne è un esempio lo spettacolare Burj Khalifa di Dubai - l’edificio più alto del mondo.
-
Xylem fornisce le pompe per il grattacielo residenziale più alto di Londra
Landmark Pinnacle è un grattacielo di 75 piani situato ai margini del distretto finanziario di Londra, Canary Wharf. Con un’altezza di 233 m, l’edificio è la torre residenziale più alta non solo di Londra, ma dell’Europa occidentale.
-
Low-pressure UV system ensures reliable and sustainable service water supply
The Böseler Goldschmaus GmbH & Co. KG site features its own modern wastewater treatment plant (38,500 ECW). To always ensure high water quality, a reliable solution was sought to keep the proportion of microorganisms, viruses, and multi-resistant germs safely below the prescribed limits without the use of chemicals.
-
New DAF Design Proves Twice As Efficient During Equipment Maintenance
An oil refinery in the US Midwest scheduled repairs to an existing wastewater treatment system. Refinery operations needed a temporary treatment system on site to maintain uptime during the outage. -
Utility transforms operations with Xylem’s Sensus advanced metering solutions
Great Lakes Energy Cooperative (GLE), Michigan’s largest member-owned electric co-op, is in the midst of a multi-year effort to modernize its operations. Serving over 130,000 members, the cooperative launched a project to upgrade its aging power line carrier (PLC) based system to the Sensus FlexNet® communication network in late 2022. -
Hong Kong: development of digital twin pilot for trunk mains water systems in selected areas of New Territories East Region
This project aims to build and calibrate a hydraulic model for trunk mains water systems in selected areas of New Territories East Region and deploy the model through Idrica’s Real-Time What-If-Scenarios solution (now called Xylem Vue).
-
Hong Kong: development of digital twins for freshwater network in selected areas of New Territories East (NTE) Region
Idrica, Xylem´s partner, has delivered its GoAigua solution (now called Xylem Vue) to the Hong Kong Water Supplies Department (WSD) as a pilot project. This deployment aims to develop a digital twin solution customized for the existing freshwater network in selected areas of its NTE Region.
-
Kentucky distillery adds DAF, MBBR for water reuse and wastewater treatment
Xylem sales and engineering teams worked with the distillery to identify wastestreams that could be reused and design a treatment system that would meet the distillery’s flow and water quality requirements.
-
Splash Lagoon: Improving uptime and efficiency with advanced filtration
Discover how Splash Lagoon, a top 10 U.S. waterpark, improved water clarity and efficiency in its 200,000-gallon wave pool using Xylem’s Defender® filtration system while cutting maintenance, conserving resources, and enhancing guest experience.