-
How B-TEC is Transforming Spray Gun Cleaning
Leveraging a custom Xylem Flojet G70 pump, B-TEC’s system ensures contamination-free, high-performance spray gun cleaning. The solution boosts reliability, speeds cleaning cycles by 50%, and supports over 20,000 global installations in precision paint environments.
-
Enhancing resilience for London’s Silvertown Tunnel, a major piece of transport infrastructure
Discover how Xylem delivered six pumping stations to prevent flooding in London’s new Silvertown Tunnel, ensuring safe, reliable transport for 25,000 vehicles daily.
-
Sazerac Northwest Ordinance Distilling (NOD) plant upgrades to sustainable anaerobic membrane bioreactor (AnMBR) system
The cost of hauling wastewater caused Sazerac Distilling to upgrade its wastewater treatment system to a sustainable anaerobic membrane bioreactor (AnMBR) system by Xylem. -
Cleaner water, smarter systems, zero disruption
Pro Club in Bellevue, Washington upgraded its pool system in seven days with advanced filtration and UV technology. The project improved water clarity, air quality, and member experience while saving over 520,000 gallons of water and $134,000 annually.
-
Xylem’s Bell & Gossett assists Massachusetts based child welfare organization in creating a healthier environment
Situated on Winter Island, a 54-acre peninsula located northeast of Salem, Massachusetts, Plummer Youth Promise is a child welfare organization that...
-
ARA Pustertal AG implementa un digital twin: risparmio energetico del 10% con il 33% in più di reflui
Le acque reflue trattate provengono per circa il 50% da attività turistiche, per il 25% da utenze municipali e per il restante 25% da scarichi industriali. Tra le principali fonti di reflui industriali si annoverano caseifici locali, un produttore di succhi e un’azienda che lavora carne e insaccati.
-
Publiacqua SpA: Integrating the drinking water management system
Centralize water cycle management for Publiacqua SpA, the utility in charge of providing the drinking water service in Medio Valdarno, in Tuscany, which has four provinces: Florence, Prato, Pistoia and Arezzo.
-
Immokalee Water & Sewer District: deployment of a comprehensive water management solution
The Immokalee Water and Sewer District was set up in 1978 to provide affordable, reliable water and sewer services to Immokalee, an unincorporated area of Collier County, Florida. The district operates and maintains the water and sewer plants and systems as an Independent Special District of the State of Florida, serving more than 24,000 year-round residents.
-
Metro Water Services: deploying a digital twin to manage drinking water distribution in real time
Nashville’s city government has a deep-rooted history in the water industry, providing drinking water to its citizens since the early 1800s. Today, Nashville Metro Water Services (MWS), Tennessee, serves more than 191,000 customers in Nashville and surrounding counties.
-
Taron™ Activated Sludge Filter Provides Effective Total Suspended Solids (TSS) Reduction
For Pennsylvania’s Western Butler County Authority (WBCA), peak flow events due to inflow and infiltration (I&I) have gone hand-in-hand with aging sewage system and treatment plant infrastructure.
-
Taron™ activated sludge filter delivers needed capacity to meet discharge limits
A food processing company’s wastewater treatment plant was struggling to meet local discharge limits and faced a hard deadline for compliance from the local authority. The problem centered on excessive solids in the effluent. To ease the hydraulic load on the existing concrete secondary clarifier and reduce total suspended solids (TSS), Xylem installed a Taron activated sludge filter.
-
An innovative project in Neustadt in Holstein
Faced with high standards for both efficiency and sustainability, Averdung and the municipal utility sought a partner capable of realizing this supply through seawater source heat pumps using Baltic Sea water.
-
Bremen's Future District: Sustainable Energy from the River
The investor set out to realize a sustainable and innovative concept that meets the demands of a contemporary urban quarter.
-
BALTEN: Implementation of an advanced business management system (ERP)
BALTEN needed to modernize its outdated infrastructure and software platforms, so it could optimize its irrigation water transportation system and improve the overall performance of its irrigation water service.
-
Xylem CoMag helps Yorkshire Water exceed phosphorous targets
Due to a projected population increase, discharges from the site were required to undergo advanced biological treatment to reduce levels of phosphorous returned to the River Aire. This requirement was part of the UK Environment Agency’s Water Industry National Environment Programme (WINEP).
-
State of the art water treatment technology for a German outdoor pool in Bernsbach
The operators wanted to use non-hazardous table salt with electrolysis for disinfection. They were also looking for a filter technology that generates low wastewater costs and can be installed in a space-saving manner.
-
Safeguarding water supplies with SmartBall
In 2020, real water loss in the town’s network peaked at 27 percent. Leaks were undermining the town’s critical water conservation efforts. Recognizing the urgency of the issue, the town is deploying innovative solutions to combat water loss and ensure a sustainable water supply.
-
Risks associated with the use of dispense gases in a food and beverage service establishment
A dispense gas is simply a pressurized gas used for dispensing drinks. The gas of choice is typically carbon dioxide (CO2), especially for carbonated drinks such as soda and beer. Carbon dioxide is commonly employed in the food service environment in a variety of equipment systems such as carbonation, refrigeration, and....
-
-
Dŵr Cymru Welsh Water, Hirwaun Water Treatment Works, Glamorgan
Dŵr Cymru Welsh Water’s Hirwaun water treatment works is a small works (5Ml/d) which treats raw water from the Penderyn upland reservoir. Treatment is by coagulation with ferric sulphate and lime, flocculation and clarification by DAF. The clarified water is dosed with lime and this is followed by first stage filtration in four rapid gravity filters, intermediate electrochlorination and orthophosphoric acid dosing, and second stage filtration in four pressure filters. Final disinfection is by electrochlorination. The original electrochlorination plant was an Evoqua OSEC® packaged unit installed over twenty years ago and had reached the end of its asset life.
-
Fighting Water Loss: Best Practices to Reduce Non-Revenue Water and Operate Sustainably
Learn best practices for leak detection, pressure management, and smart metering to help utilities address Non-Revenue Water and move toward a more sustainable "watertight" future. This guide offers practical solutions and valuable insights to create a more efficient and equitable water infrastructure.
-
Our 15 most frequently asked questions on improving aquaculture
To help companies protect against waterborne infection and disease, Evoqua recently hosted a webinar dedicated to understanding and improving water quality in land-based hatcheries that you can watch here.
-
City of Tulare celebrates 25 years of converting waste-to-energy
The City of Tulare, located in California’s world renowned San Joaquin Valley, is known for its rich agricultural and dairy industries. Tulare is home to six large-scale cheese and dairy producers. Like many municipalities, the city is challenged to meet industrial requirements at a reasonable cost while maintaining harmonious relationships with the surrounding community.
-
CoMag® System Provides Immediate Results
Situated in Staffordshire in the UK, the Severn Trent Cannock wastewater treatment facility serves a population of 65,053. The plant had early obligation AMP7 requirements to meet for controlling phosphorus levels.