検索結果
-
-
Clayton County, Georgia reduces apparent water loss & identifies one million in recoverable revenue
Clayton County Water Authority (CCWA) is a good example of a utility that doesn’t let a confined geographical footprint stop it from thinking outside the box. As one of Georgia’s smallest counties in terms of land size area (only 143 square miles), its location near the top of a regional watershed means it has little area to gather precipitation into streams and rivers.
-
Common residential wastewater myths demystified
In most cases, bigger is not better when it comes to residential wastewater pumps. Whether a residential system requires an impeller or grinder pump, the pump should be sized for the application.
-
-
Complex Discharge Line Bypass at National Brewery Keeps Operations Online
A national beer brewery in Georgia needed to address deterioration and replacement of some of the drain pipes running from their fermentation tanks. For this to be classified as a successful repair and replacement effort, it needed to be achieved while keeping 25,000 barrels of beer a day flowing and simultaneously maximizing plant uptime and profitability.
-
-
Cover helps community control odors from wastewater treatment
When the affluent, new home development was being established, odor control was top of mind. The wastewater treatment plant was in close proximity to the new development, which includes 900 acres (364 hectares) of preserved open space, including 24 miles (38 kms) of trails, 10 neighborhood parks, a community pool and water park, as well as outdoor sport courts.
-
-
Delivering cost-effective process monitoring for the welding industry
Discover how Sentec engineered a compact, non-intrusive smart connector to digitally transform welding operations. From non-contact wire speed sensing to seamless Bluetooth integration, this case study highlights a scalable solution built for regulation, reliability and industry-wide adoption. -
-
-
Efficiency Gained Through Automated Aeration Control with a Pulse
For many years, maintaining efficient aeration control was a challenge for the 24 MGD Muncie, Indiana, Water Pollution Control Facility (WPCF). A manually operated system combined with severe mixing-limited conditions resulted in over-aeration and wasted energy. The plant alleviated this problem with automated control and Pulsed Aeration, allowing it to satisfy the needs of the bacteria and mix basin contents while expending less energy.
-
Electric Generating Station Maximizes Plant Efficiency
Xcel Energy is a leading provider of electricity and natural gas to customers in the Midwestern US. As part of their expansion plans for the Comanche Station, a coal-fired electric generating station located in Pueblo, CO, Xcel Energy contacted Evoqua Water Technologies to explore cost effective solutions for their water treatment needs.
-
EMALCSA: implementation of a digital twin to support decision-making in water supply network operations
The Empresa Municipal de Aguas de La Coruña (EMALCSA) manages the water cycle in the city of A Coruña and seven neighboring municipalities, serving a total population of 400,000. The utility collects, treats and distributes over 36 million cubic meters of drinking water to 138,000 customers each year, via a network of over 560 kilometers, 26 storage tanks and six pumping stations. -
EMASA: improving water efficiency through smart water balance analysis
EMASA (Empresa Municipal Aguas de Málaga S.A.) is the Malaga City Council’s public utility which has been in charge of managing the entire urban water cycle since 1987. The company serves more than 600,000 residents and supplies approximately 42 hm³ of drinking water. The system operates at a flow rate of up to 2 m³/s, ensuring urban water supply through an extensive pipeline network of around 2,000 km, divided into approximately 240 DMAs (District Metered Areas) and equipped with over 240,000 meters, 170,000 of which are smart devices. -
-
-
Enhancing resilience for London’s Silvertown Tunnel, a major piece of transport infrastructure
Discover how Xylem delivered six pumping stations to prevent flooding in London’s new Silvertown Tunnel, ensuring safe, reliable transport for 25,000 vehicles daily.
-
EnviroMix AquaBlend delivers high-quality drinking water in Montana
Learn how the Montana Law Enforcement Academies used EnviroMix AquaBlend™ technology to prevent water stagnation, reduce maintenance, and improve potable water quality in elevated storage tanks. -
EnviroMix BioMix enhances BNR and reduces DO in Orlando, FL
See how Orlando’s Water Conserv II WRF improved denitrification by replacing diffused-air mixing with EnviroMix BioMix to lower dissolved oxygen in anoxic basins, reduce long-term O&M costs, and strengthen BNR performance and resiliency after high-flow events. -
EnviroMix BioMix helps HRSD keep Chesapeake Bay clean
Read how HRSD used EnviroMix BioMix™ technology to improve biological nutrient removal, increase operational flexibility, and reduce O&M costs at the VIP Wastewater Treatment Plant. -
EnviroMix BioMix minimizes maintenance for WI cheese maker
Read how Mullins Cheese used EnviroMix BioMix™ technology to reduce maintenance, optimize aeration control, and improve mixing efficiency in its wastewater treatment process. -
EnviroMix BioMix provides O&M savings in Russellville, AR
See how Russellville’s Pollution Control Works reduced operating costs with BioMix compressed gas mixing and achieved 75% energy savings in Phase I and more than 60% in Phase II versus mechanical mixers. -
EnviroMix BioMix reduces energy and maintenance in Broomfield, CO
See how Broomfield’s Wastewater Reclamation Facility improved thickened sludge holding tank mixing with EnviroMix BioMix and reduced energy use by more than 50% versus coarse bubble aeration, saving about $10,000 annually.