It looks like you are coming from United States, but the current site you have selected to visit is Japan. Do you want to change site?
As consumer demand for milk, cheese, and related by-products continues to grow, the dairy processing industry relies on Xylem for more versatile, cost-effective ways to spray, disinfect, transfer and produce dairy products across the entire value chain.
A high level of teat hygiene, pre- and post-milking, is essential to maximize milk volume, quality and herd health. Flojet pumping solutions work with a wide range of products and both their compact size and long life make them an ideal choice for the system builder.
Keeping your dairy equipment clean is necessary as it ensures that not only the milk quality is maintained, but also that the life of the dairy equipment is prolonged. Flojet offers a wide range of reliable pumping solutions to ensure that your needs are met.
Flojet pumps are used in milk transfer applications around the dairy, transporting mixed or fresh milk to calf feeding stations. These durable long-life pumps with anti -clog stainless steel impellers are well suited to the application.
Modern dairy farms rely on automation to ensure productivity, and that includes cleaning up the manure. Flojet diaphragm pumps are ideal pumps for spraying a powerful jet of water to break up dirt ready for collection.
For many in the food industry, pumping delicate, viscous fluids and products that contain solids in suspension has been a daily challenge. There are many types of pumps on the market; however the effects on product quality can be disastrous if the wrong type of pump is installed in the process. Jabsco Flexible Impeller Pumps (FIP) offer significant benefits when compared to other pump types for the pumping of viscous foodstuffs and other fluids that contain fragile solids.
Modern milk tankers rely on large centrifugal pumps for the flow rates needed for fast filling and emptying, however these pumps have an inability to self prime or to scavenge the last drops of milk. Jabsco flexible impeller pumps are the ideal complementary pump for use on this type of tanker.
ご連絡いただきありがとうございます。 担当者よりご連絡を差し上げます。
All fields required.