It looks like you are coming from United States, but the current site you have selected to visit is Japan. Do you want to change site?
Unlike a car motor, boat engines use the cool water from below the vessel to keep cool. There are two main types of marine cooling systems that boat engine manufacturers install on a boat. A raw water cooling system sucks the water in through a strainer and then cycles it through the engine block. That water then usually exits through the exhaust and out the back or below the boat. A closed-loop cooling system runs water through a series of heat exchangers, which avoids having any raw saltwater inside through the engine block.
Jabsco engine cooling pumps have a long tradition of innovation, and are engineered to effectively cool your engine, which results in better engine performance and fuel economy. With their rugged, compact, reliable design, good flow and wear-resistant impellers, these tough, long-lasting pumps are used in a wide range of marine cooling solutions that include heat exchanger cooling systems, keel cooling systems, and direct cooling systems. So whether you're offshore or at the dock, you can choose from a range of different sizes, mounts, and marine quality bronze and stainless-steel constructions.
インペラポンプの内部構造と仕組みをご覧ください
インペラプーラーを使い、インペラを簡単に取り外す方法をご紹介します。
ご連絡いただきありがとうございます。 担当者よりご連絡を差し上げます。
All fields required.