您似乎来自United States,但您选择访问的当前网站是China。是否更换网站?

是,请更换! 否,停在当前网站。

Enable high contrast mode

Operation

Download the device documentation

The device documentation represents the device specification used in Secure Connect.

  1. Navigate and login into OPC UA Connector WebUI.
  2. In the top menu, click Documentation.
  3. Select document from the dropdown.
  4. Click the Open button to download the file

Enable anonymous OPC UA user access

Anonymous OPC UA User Access will allow OPC UA Read or Read/Write permissions for unauthenticated users.

  1. Navigate and log in to OPC UA Connector WebUI.
  2. In the top menu, select Users.
  3. Click the Anonymous access.
  4. Select Read or Read/Write to set permissions for anonymous access.
  5. Click the Save button.