It looks like you are coming from United States, but the current site you have selected to visit is Equatorial Guinea. Do you want to change site?

Yes, please! No, keep me on the current site

  • UNA EXPERIENCIA INCOMPARABLE

    Insuperables en materia de achique

    Tanto si bombea agua limpia, lodos, purines o líquido con niveles extremos de pH, contamos con la bomba y los accesorios adaptados a sus necesidades.

  • UNA EXPERIENCIA INCOMPARABLE

    Insuperables en materia de achique

    Tanto si bombea agua limpia, lodos, purines o líquido con niveles extremos de pH, contamos con la bomba y los accesorios adaptados a sus necesidades.

  • UNA EXPERIENCIA INCOMPARABLE

    Insuperables en materia de achique

    Tanto si bombea agua limpia, lodos, purines o líquido con niveles extremos de pH, contamos con la bomba y los accesorios adaptados a sus necesidades.

Do you need to address an operational emergency?

With Xylem’s comprehensive rental solutions, you can solve even the most difficult water and wastewater challenges.

At Xylem we rent out more than just pumps and treatment systems. We offer world-class expertise to provide you with cost-effective, reliable and innovative full-service solutions for even the most complex applications – tailor-made for the specific needs of your business

Tell us about your needs and we will deliver the right solution to you.

Proximity:

With over 50 rental points in Europe we are close to you. Europe’s largest rental bank & local expertise, we serve all water-related challenges at the highest standards across the continent.

Our extensive regional service network guarantees fast assistance.

Find your local Site

Expertise:

Anybody can rent a pump, including us. What sets us apart is being the Original Equipment Manufacturer (OEM) along with the depth of our experience, the comprehensive range of design services, the breadth of our fleet, and our unrivalled ability to solve the biggest, most complex water challenges.

Availibility:

At Xylem, we do more than renting only equipment. We offer in-depth application expertise to provide cost-effective, reliable, innovative solutions to even the most complex transient water challenges specific to your industry.

Rental Solutions for All Water Related Issues:

Maintain infrastructure whithout interruption of the service

Water and wastewater infrastructure suffer wear and tear due to internal and external factors such as corrosion, pressure surges etc., and consequently need repair and maintenance to continue operating at peak performance. Shutting down critical infrastructure to carry out repairs is not often a feasible option, making a temporary bypass necessary to avoid operational disruption while rehabilitating the pipe network.

 

Address emergencies safely

Sometimes, environmental events such as heavy rains, floods etc. can also overwhelm the existing infrastructure, necessitating a bypass implementation as a “safety valve” to mitigate negative consequences related to system overload.

 

Services from Xylem EU Rental Hub

EU Rental Hub Case studies:

Xylem helps pulp & paper producer meet EU wastewater discharge regulations with containerized Ozone

Xylem’s containerized Ozone treatment solution helps a pulp & paper producer in Italy to meet EU wastewater discharge regulations while ensuring high availability to support the continuous operation of the bleaching line

Learn how Xylem’s disinfection solutions can help address flood mitigation and ensure safe discharge

Xylem’s containerized Ozone treatment solution helps a pulp & paper producer in Italy to meet EU wastewater discharge regulations while ensuring high availability to support the continuous operation of the bleaching line.

Xylem delivers complex turnkey bypass to facilitate sewer connection project in France

To address the ageing infrastructure of a French municipality, Xylem delivers a turnkey sewer bypass to test and bring online a new wastewater treatment plant without operational disruption during the switchover from the old facility to the new facility.

Industries served by Xylem Rental Services:

We specialize in solutions for your raw water intakes, wastewater, and storm water needs across a wide range of industries. Xylem Rental Solutions offers temporary or long-term rental equipment for your industrial needs including: hydrostatic testing, lift station backup pumping, storm and process sewer bypass, process water supply, intake inspections, zebra mussel removal, cooling tower supply and circulation, basin ballasting, sludge removal, slurry tailings removal, and temporary fire protection.

Marine

Marine environments are harsh. Shutting down is not an option, so the equipment selected must be rugged and proven reliable. Xylem Rental Solutions equipment, paired with process engineering expertise, provides solutions that are energy efficient, effective, and most of all, reliable. Our temporary equipment can be used for: barge ballasting, jetting, temporary fire protection, vessel dewatering, and recovery.

Food and Beverage

With global population continuing to grow, feeding the world sustainably is a worldwide challenge. As a leading OEM in the water industry, we deliver solutions covering the entire water cycle that are energy efficient, reliable and tailored for your unique challenges in the food & beverage industry.

Pulp & Paper

Water is crucial to pulp and paper manufacturing. And regardless of your mill’s water footprint, our industrial experts will help you optimize each aspect of the water cycle. We can integrate your operations from influent to process water to reuse – and everything in between – to reduce costs, better protect the environment and turn water management from an expense to a strategic advantage.

Agriculture

Xylem Rental Solutions pumps, mixers and other water and sludge handling systems can meet both temporary and long-term needs and are designed to irrigate every part of your field. With products that stand tough in the harshest environments, we listen, learn and adapt to your local environment, helping your agricultural operations thrive without interruption.

Mining

From open pit and underground, to face and stage dewatering, to slurry tailings removal to camp and process water supply, Xylem Rental Solutions has the right product and application support to help you efficiently and reliably manage the water challenges associated with all types of mining all over the Americas.

Oil & Gas

Whether upstream, midstream or downstream, we understand that water is a critical and costly input to the oil and gas industries. Xylem Rental Solutions offers both temporary and long-term rental equipment for: drill rig water supply, hydrostatic testing, pipeline pigging, product transfers in refineries, temporary cooling and process water pumps, fire protection systems, pipeline anomaly and corrosion repair dewatering, and pipeline crossing diversions of any size – with the ability to remotely monitor and control all of Xylem’s rental assets on your project.

Power Utilities

We understand that power plants require reliable flows for cooling water, raw water intakes, condensation, auxiliary water, makeup water, and temporary fire protection systems. We also understand that pump failure is not an option as it can lead to power plant shutdowns. Whether you’re facing a planned outage or require emergency response, Xylem Rental Solutions has the equipment and experience to assist in keeping your assets on line and manage environmental impact. Xylem Rental Solutions can also help you meet demanding specifications for low discharge velocities to avoid scouring, and remote monitoring of total suspended solids at your discharge locations.

Marine

Marine environments are harsh. Shutting down is not an option, so the equipment selected must be rugged and proven reliable. Xylem Rental Solutions equipment, paired with process engineering expertise, provides solutions that are energy efficient, effective, and most of all, reliable. Our temporary equipment can be used for: barge ballasting, jetting, temporary fire protection, vessel dewatering, and recovery.

Food and Beverage

With global population continuing to grow, feeding the world sustainably is a worldwide challenge. As a leading OEM in the water industry, we deliver solutions covering the entire water cycle that are energy efficient, reliable and tailored for your unique challenges in the food & beverage industry.

Pulp & Paper

Water is crucial to pulp and paper manufacturing. And regardless of your mill’s water footprint, our industrial experts will help you optimize each aspect of the water cycle. We can integrate your operations from influent to process water to reuse – and everything in between – to reduce costs, better protect the environment and turn water management from an expense to a strategic advantage.

Agriculture

Xylem Rental Solutions pumps, mixers and other water and sludge handling systems can meet both temporary and long-term needs and are designed to irrigate every part of your field. With products that stand tough in the harshest environments, we listen, learn and adapt to your local environment, helping your agricultural operations thrive without interruption.

Mining

From open pit and underground, to face and stage dewatering, to slurry tailings removal to camp and process water supply, Xylem Rental Solutions has the right product and application support to help you efficiently and reliably manage the water challenges associated with all types of mining all over the Americas.

Oil & Gas

Whether upstream, midstream or downstream, we understand that water is a critical and costly input to the oil and gas industries. Xylem Rental Solutions offers both temporary and long-term rental equipment for: drill rig water supply, hydrostatic testing, pipeline pigging, product transfers in refineries, temporary cooling and process water pumps, fire protection systems, pipeline anomaly and corrosion repair dewatering, and pipeline crossing diversions of any size – with the ability to remotely monitor and control all of Xylem’s rental assets on your project.

Power Utilities

We understand that power plants require reliable flows for cooling water, raw water intakes, condensation, auxiliary water, makeup water, and temporary fire protection systems. We also understand that pump failure is not an option as it can lead to power plant shutdowns. Whether you’re facing a planned outage or require emergency response, Xylem Rental Solutions has the equipment and experience to assist in keeping your assets on line and manage environmental impact. Xylem Rental Solutions can also help you meet demanding specifications for low discharge velocities to avoid scouring, and remote monitoring of total suspended solids at your discharge locations.

Contacte con nuestros expertos

¿Tienes un proyecto? ¿Una necesidad específica? ¡No dude en enviarnos su solicitud!

All fields required.

*  Required Field