Documents
-
Temporary DAF system supports refinery outage
A temporary wastewater treatment system was deployed during a planned outage to support operations while two existing DAF units underwent repair. -
-
Soil and groundwater remediation
Soil and groundwater remediation projects often call for treatment of groundwater, soil vapor extraction condensate, soil vapor and other liquid and vapor streams for removal of volatile and semi volatile organic compounds. Xylem's Carbonair has provided thousands of STAT Low Profile Air Strippers, liquid phase and vapor phase carbon vessels for remediation systems over our 30 plus years in business.
-
-
Southern California water utility consults Xylem for disinfection of potable water
Located in Southern California, this water utility uses wells to store water. These same wells are also used for fire protection. which is especially critical during the summer months. The supply covers about 10,000 customer connections with chloraminated water for residual disinfection, with chlorine and ammonia boosting in various locations.
-
Specification Tips to Maximize Heat Transfer: Shell and Tube
Heat exchangers are widely used in various industries including chemical, oil & gas, power generation, food & beverage, HVAC & refrigeration, pulp & paper to name a few, and are expecting strong growth over the coming years driven in part by a rising focus on environmental impact and improving efficiency standards.
-
-
Stadtwerke Trier: AI-aided energy optimization for daily energy balancing
Xylem Vue helped Stadtwerke Trier optimize renewable energy use in its drinking water network, achieving 90% self-consumption. -
Supervision of pumping stations in Vlaardingen is highly effective
In the municipality of Vlaardingen, rainwater and wastewater are processed by more than seventy pumping stations, six of which are large, dry-installed main pumping stations and a large number of subsidiary and mini-pumping stations. Supervision is the responsibility of Xylem, which means that the Vlaardingen maintenance department receives a weekly overview of all relevant events.
-
-
-
Taron™ activated sludge filter delivers needed capacity to meet discharge limits
A food processing company’s wastewater treatment plant was struggling to meet local discharge limits and faced a hard deadline for compliance from the local authority. The problem centered on excessive solids in the effluent. To ease the hydraulic load on the existing concrete secondary clarifier and reduce total suspended solids (TSS), Xylem installed a Taron activated sludge filter.
-
-
Temporary pumping ensures continuous service during asset replacement
After an unexpected wastewater pump failure, Xylem rapidly installed a temporary NC200 Electric unit integrated with the site’s existing pipework, power and controls to maintain uninterrupted operation during the replacement lead time. Variable speed control and 24/7 Secure Connect monitoring ensured efficient, reliable performance throughout the extended hire period, even when a second pump failed. -
-
-
-
The Smarter Water Manager
Communities around the world are facing a growing storm. Complex challenges including water scarcity, changing demographics, extreme weather patterns, and aging or overly stressed infrastructure are colliding to threaten critical water, energy, transport, enterprise and health networks. The water industry is in the eye of the storm.
-
Intelligent wastewater pumping eliminates clogging and cuts energy use at Heathrow Airport
Flygt Concertor was trialed at Heathrow Airport to solve chronic clogging and delivered clog-free pumping while cutting energy use by 53%.
-
-
Town of Creston Pretreats Brewery Wastewater with ADI-BVF® Reactor
Creston’s wastewater treatment facility treats both domestic and industrial effluent. The Columbia Brewery, which feeds its wastewater to the town, underwent major expansions that significantly increased its wastewater flows. Creston was not equipped to treat the volume of wastewater generated by the brewery. Town officials were eager to solve the problem, especially since the brewery was Creston’s largest employer.
-
-
Turnkey solution eliminates chain and scraper downtime in Grass Valley, CA
The Grass Valley Wastewater Treatment Plant provides service for a population of approximately 12,000 people. Situated in California’s Gold Country, the area has some unique challenges that include mine drainage and heavy flows during the winter storm season in the scenic Sierra Nevada foothills. On average, the City discharges 2.1 million gallons per day of treated wastewater effluent to Wolf Creek, a tributary of the Bear River.
-